• Products and Partners
    Products and Partners
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
Member's Forum I am looking for some help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 5 answers
  • Subscribers 632 subscribers
  • Views 2157 views
  • Users 0 members are here
Related

I am looking for some help

jlusco
jlusco over 8 years ago

I am newer to DIY electronics and I am working on a project. I have a project that I am building and I am stuck on this one part. I have an Adafruit Mono 2.5W Class D Audio Amplifier - PAM8302 and I want to bring teh Speaker out to another board that will have a Speaker and headphone jack on it. I want to wire it so when the headphones are plugged in the speaker is off and the sound comes through the headphones but when unplugged the sound comes out the speaker. Below is a basic mock up of what I want and I am just stuck on how to accomplish it.

I have tried to Google the answer but have had no luck. Orange dots are the thru hole solder points for each component any help will be appreciated.

 

 

MockUp

  • Sign in to reply
  • Cancel
Parents
  • genebren
    0 genebren over 8 years ago

    Jacob,

     

    The connections are really quite simple.  The diagram below is how it should work.  Keep in mind that the pin-out on the headphone jack will need to match the part that you are using.

     

    image

    Good luck,

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jlusco
    0 jlusco over 8 years ago in reply to genebren

    So can this audio amp be connected to the Raspberry Pi Zero without using the GPIO. Can I solder the Vin, GND, A+, and A- to the USB Test Pads and use it to get sound?

     

    Adafruit Mono 2.5W Class D Audio Amplifier - PAM8302

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to jlusco

    Jacob,

     

    Not quite sure that I know what you are trying to do here. Best I can tell, Vin and Gnd are your power supply connections (2.5V to 5.5V), SD is used to turn the amp 'on' (Vin) or 'off' (gnd).  A+ and A- are your inputs (differential, if single-ended use A+ and tie A- to gnd.

    How this relates to the USB Test Pads is where I am getting lost.

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ifish
    0 ifish over 8 years ago in reply to jlusco

    Hi Jacob,

     

    I think your misinterpreting that table as only GPIO0-27 are available by way of the 40 pin header, its a bit confusing but there are two ways of referencing the pins on the 40 pin header.  If you look at the schematic symbol you have posted each pin has a pin number and a description associated to it, pin 40 is in fact GPIO 21.

     

    image

    Which if we look at your table you have linked to isn't capable of being used for PWM

    image

     

    After looking the link you posted I get the feeling the guy used a USB audio device rather then the IO, but if you don't need two sets of triggers you could use GPIO 18 (pin 12) and wire you amplifier to this pin and ground.  You'll need to make some software modification, according to Step 7 of the projects setup (https://github.com/32teeth/Gameboy-Zero-Kickstarter/blob/master/INSTALL.md ) you have to edit the control setup anyways.  You'll want to free up gpio 18, so delete the following two lines from the config file

     

    A 18  # Left shoulder button

     

    OR

     

    change

    A 18  # Left shoulder button

    to

    A 21  # Left shoulder button

     

    but doing this will require you to lift the tact switch from being connected to GPIO_18 and run a wire from the tact switch to the GPIO_21.

     

    Hope this helps

    Chris

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ifish
    0 ifish over 8 years ago in reply to jlusco

    Hi Jacob,

     

    I think your misinterpreting that table as only GPIO0-27 are available by way of the 40 pin header, its a bit confusing but there are two ways of referencing the pins on the 40 pin header.  If you look at the schematic symbol you have posted each pin has a pin number and a description associated to it, pin 40 is in fact GPIO 21.

     

    image

    Which if we look at your table you have linked to isn't capable of being used for PWM

    image

     

    After looking the link you posted I get the feeling the guy used a USB audio device rather then the IO, but if you don't need two sets of triggers you could use GPIO 18 (pin 12) and wire you amplifier to this pin and ground.  You'll need to make some software modification, according to Step 7 of the projects setup (https://github.com/32teeth/Gameboy-Zero-Kickstarter/blob/master/INSTALL.md ) you have to edit the control setup anyways.  You'll want to free up gpio 18, so delete the following two lines from the config file

     

    A 18  # Left shoulder button

     

    OR

     

    change

    A 18  # Left shoulder button

    to

    A 21  # Left shoulder button

     

    but doing this will require you to lift the tact switch from being connected to GPIO_18 and run a wire from the tact switch to the GPIO_21.

     

    Hope this helps

    Chris

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer