Member's Forum LED Construction
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 629 subscribers
  • Views 1021 views
  • Users 0 members are here
  • light-emitting diode
  • electroluminescence
  • led
  • active region
Related

LED Construction

Anonymous-532400
Anonymous-532400 over 8 years ago

Hello,

I was researching how an LED works, and came across two things that I can't seem to find any solid information on, the "active region", and the "substrate" of an LED.

So, if anyone could explain a little what these are and what they do, that would be appreciated.a

 

Light Emitting Diodes

  • Sign in to reply
  • Cancel
Parents
  • DAB
    0 DAB over 8 years ago

    Hi Nicholas,

     

    WARNING I have an alternative view of electronics.

     

    Now, if you are still reading, I have been doing some research into subatomic physics and have concluded that it is photon flow, not electron flow that makes everything in the universe work.

     

    For you questions, the Substrate is usually a piece of silicon on which the specific semiconductor is constructed. In most cases this is "pure" silicon.

     

    The active region is another piece of silicon in which specific "doping" atoms are added to the crystal structure to create areas where current flow is easy or current flow is inhibited.

     

    From my theory, the doping atoms create areas within the crystal matrix where photons flow differently than they do for the silicon atoms. This natural flow of photons reduces the resistance of the silicon substrate so that it facilitates photon flow when a bias voltage is applied to the junction.

     

    The LED "light" is emitted at the junction between the substrate and the active region itself.

     

    Again, my view is that the transfer of photons across the different silicon material results in specific types of photons to be released by the atoms as other photons flow between the atoms. Essentially the doping atoms behave very predictably under these conditions to free of photons of a narrow range of frequencies, which is by you get emission of Red, Blue, Green, Yellow, UV or IR wavelengths. The only thing that changes is the type of doping material and the density of the doping atoms.

     

    In most cases, each LED also emits an IR component. In some cases the manufacturer will put an IR blocking filter inside the LED so that only the visible light photons escape.

     

    Conventional theory will tell you that the photons are emitted because the electrons are changing orbital levels around each doping atom. I dispute this view because nobody has ever proven that electrons can orbit an atom let alone change energy levels by the absorption or emission of photons. My work has demonstrated that each atom is really surrounded by a very large number of captured photons, which when voltages are applied across these atoms some of the captured photons are emitted while other photons are absorbed by each atom.

     

    Either way, the light does come out of the LED at very specific frequencies.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 8 years ago

    Hi Nicholas,

     

    WARNING I have an alternative view of electronics.

     

    Now, if you are still reading, I have been doing some research into subatomic physics and have concluded that it is photon flow, not electron flow that makes everything in the universe work.

     

    For you questions, the Substrate is usually a piece of silicon on which the specific semiconductor is constructed. In most cases this is "pure" silicon.

     

    The active region is another piece of silicon in which specific "doping" atoms are added to the crystal structure to create areas where current flow is easy or current flow is inhibited.

     

    From my theory, the doping atoms create areas within the crystal matrix where photons flow differently than they do for the silicon atoms. This natural flow of photons reduces the resistance of the silicon substrate so that it facilitates photon flow when a bias voltage is applied to the junction.

     

    The LED "light" is emitted at the junction between the substrate and the active region itself.

     

    Again, my view is that the transfer of photons across the different silicon material results in specific types of photons to be released by the atoms as other photons flow between the atoms. Essentially the doping atoms behave very predictably under these conditions to free of photons of a narrow range of frequencies, which is by you get emission of Red, Blue, Green, Yellow, UV or IR wavelengths. The only thing that changes is the type of doping material and the density of the doping atoms.

     

    In most cases, each LED also emits an IR component. In some cases the manufacturer will put an IR blocking filter inside the LED so that only the visible light photons escape.

     

    Conventional theory will tell you that the photons are emitted because the electrons are changing orbital levels around each doping atom. I dispute this view because nobody has ever proven that electrons can orbit an atom let alone change energy levels by the absorption or emission of photons. My work has demonstrated that each atom is really surrounded by a very large number of captured photons, which when voltages are applied across these atoms some of the captured photons are emitted while other photons are absorbed by each atom.

     

    Either way, the light does come out of the LED at very specific frequencies.

     

    DAB