• Products and Partners
    Products and Partners
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
Member's Forum Need some guru help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 631 subscribers
  • Views 806 views
  • Users 0 members are here
Related

Need some guru help

joshuastovall
joshuastovall over 8 years ago

Sorry if this ended up in the wrong area but i need some help from some knowledgeable people. I am trying to repair my tv. I have identified three capcitors that are the problem they are blown but im not sure what to shop for. Can someone point me in the right direction of what to buy?  Pics posted the side by side ones look to be the same marks the one by itself i think its a different one.

 

My soldering skills are good but never got the chance to take classes to learn more. So im comfortable doing the repairs just not sure what to buy or where to buy them.

 

Thanks any help is appriciated.

Fullscreen contentimage_147941.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    0 Gough Lui over 8 years ago

    How did you determine the capacitor needs replacement? You may be right, but sometimes it's good to keep in mind that there may be other things that can be wrong. Another is that the safety of tinkering with such equipment - capacitors can hold a charge that can be unpleasant through to even lethal.

     

    From your image, which is very blurry, it looks like a Samyoung 820uF 250V electrolytic capacitor rated at 105 degrees C (in brown). Ultimately, if this is the part you want to replace, then it's good to purchase a low-ESR capacitor of an equivalent 820uF rating and a voltage rating of at least 250V. Changing with another unit that comes from a reputable brand is highly recommended (e.g. Panasonic, Rubycon, ELNA, Nippon-Chemi-Con, Nichicon or Sanyo). You will need to check the spacing between the legs and the height of the can if it's a tight fit.

     

    Likewise, perhaps try taking a clearer photo - use the Macro mode on your camera if you can. When dealing with mains, be careful - any mistake could be disastrous. Electrolytic capacitors are polarized - get them in the wrong way around and you will ... have some loud noises and magic smoke.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 8 years ago

    How did you determine the capacitor needs replacement? You may be right, but sometimes it's good to keep in mind that there may be other things that can be wrong. Another is that the safety of tinkering with such equipment - capacitors can hold a charge that can be unpleasant through to even lethal.

     

    From your image, which is very blurry, it looks like a Samyoung 820uF 250V electrolytic capacitor rated at 105 degrees C (in brown). Ultimately, if this is the part you want to replace, then it's good to purchase a low-ESR capacitor of an equivalent 820uF rating and a voltage rating of at least 250V. Changing with another unit that comes from a reputable brand is highly recommended (e.g. Panasonic, Rubycon, ELNA, Nippon-Chemi-Con, Nichicon or Sanyo). You will need to check the spacing between the legs and the height of the can if it's a tight fit.

     

    Likewise, perhaps try taking a clearer photo - use the Macro mode on your camera if you can. When dealing with mains, be careful - any mistake could be disastrous. Electrolytic capacitors are polarized - get them in the wrong way around and you will ... have some loud noises and magic smoke.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • joshuastovall
    0 joshuastovall over 8 years ago in reply to Gough Lui

    The tops are buldging on them. Cant see it in the photo but when you look at them across the tops it is obvious. As well as they make a clicking sound when pressed on top. No power is getting past the board to the other boards in the circuit. Everything else looks fine. The rest of the capacitors look to be in great shape considering its an 11 year old tv.

     

    Tested the output from the board to the others with one of those pointy curcuit tester probe things with the light bulb inside. It worked with a 5v source (usb cord) so i figured it could tell me if power is being pushed to the other boards.

     

    Thanks for the warnings. Im comfortable doing the repairs i just dont know what im looking for shopping wise. I put in the specs in google and keep getting A/C capacitors. Or ones that look too small.

     

    I never learned any of the formal stuff like the measurements terminology or the like. I got into soldering years ago building those robot kits from radio shack.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to Gough Lui

    For example, you could do a search on Element14 for Aluminium Electrolytic Capacitor, filtered by 820uF and 250V rating:

    https://au.element14.com/c/passive-components/capacitors/aluminium-electrolytic-capacitors?capacitance=820uf&voltage-rat…

     

    (Link above is to the Australian element14 arm, but you can do the same for your own local distributor).

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer