I do struggle with making sure I understand what a data sheet is telling me so I'm hoping someone can confirm or otherwise explain my understanding of something. I'm looking at the data sheet for a LTC1624 - http://www.farnell.com/datasheets/1713911.pdf?_ga=2.75130708.790743949.1554834791-441347304.1541859637&_gac=1.136456708.1554891125.EAIaIQobChMI16fD9tLD4QIVz5TtCh3QQglqEAAYAiAAEgKKrvD_BwE
The electrical characteristics state that Vfb feedback current is typically 10nA, max 50nA; Vfb feedback voltage is min 1.178v to max 1.20v.
I'm trying to analyse a circuit, not dissimilar to that shown as an example application in the data sheet, and have built it up in LTSpice. When I simulate this, I can see voltage going into the Vfb pin of 1.15v to 1.3v with peaks of 1.8v falling down to 1.3v (this is a switching regulator at 200Khz). I can see current at the Vfb pin of 14.75nA with peaks of -130nA and 110nA. It will swing from 14nA to -130nA to 110nA back to 14nA in a period of 0.02ms.
This can vary significantly with output load (the above is with a 1kohm load and is more extreme with lower resistance.) If I build the example application in the data sheet the current to the Vfb pin is within the specified range but the voltage is under the minimum level or over the maximum (again, depending upon load.)
My assumption would be that my circuit would be a problem but it's confusing because the example application also simulates outside the specifications. This is when I start to think I'm not interpreting the data sheet information correctly. Could someone proffer some advice?
I've not posted pictures of the circuit or the simulation results because it's more a question of correctly/incorrectly interpret the specifications - obviously I can if it's important/useful enough.
Thanks
Andrew