• Products and Partners
    Products and Partners
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
Member's Forum Testing a Mosfet and Schottky in-circuit; Bit more advice
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 27 answers
  • Subscribers 630 subscribers
  • Views 8918 views
  • Users 0 members are here
Related

Testing a Mosfet and Schottky in-circuit; Bit more advice

Andrew J
Andrew J over 7 years ago

I presume this is possible with power off, looking for resistance between drain and source?

 

I'm pretty sure I've killed it - resistance is 0.33Ohms between these two pins image  Out of circuit, on a good one, it is > 13MOhms.  Looking at my circuit, I've solder the Schottky Rectifier the wrong way around - cathode to ground imageimageimage  Pretty sure that won't have done the Mosfet any good, it was too hot to touch.  Can't believe I've been so stupid - by good luck, rather than management, the other Schottky I have in the circuit (not shown below) is the right way around.

 

Is there a way of testing the Schottky rectifier in-circuit - I've tried it and the DMM 'beeps' as it detects a normal junction; measures 0.159v and 0.579V depending upon orientation of test leads?  Just to clarify - in the schematic below you can see how the Schottky rectifier should be - however, as I say, it's actually reversed and I don't know if that might affect readings. So, with the COM lead to the cathode and test (red) lead to anode it reads 0.159v; with the COM lead to the anode and test (red) lead to cathode it reads 0.579V.  I can test one out of circuit and I get 0.157V and OL respectively.  I think that indicates it is ok but in circuit it isn't reading as OL: I have to remove it to swap it around in any case so would the advice be to chuck it and use a new one? 

 

I'm really hoping I can get it off with wick and an iron and without damaging the board; ditto the Mosfet. I really don't want to lump out for a rework station.

 

Is there likely to be damage to other components down stream?  Any tips for testing components without removing them from the circuit?

 

This is only part of the circuit but shows the relationship between the Mosfet and Schottky rectifier:

 

image

 

[silently screaming inside]

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    0 jc2048 over 7 years ago

    Resistance reading in-circuit is difficult because of paths round through the power and through the ICs [via the protection circuits]. You'll tend to see initially low readings that move because you're charging decoupling capacitors. I don't like doing it because of the possibility of damage to chips [a handheld meter is probably worse than a good bench meter in that respect], but then I tend to be very over-cautious.

     

    Commercially, you'd chuck the components and use new ones (the parts cost is much, much lower than the cost to you of a person messing around with parts that are suspect). Actually, you might well label the board carefully, put it to one side, and move to the next, unused prototype, unless there were good reasons for sticking with the same one.

     

    For a personal project it's different and you may want to experiment a bit. The MOSFET and Schottky are fairly robust. Just because you can't bear to touch it doesn't mean it is dead. The controller is working current mode, monitoring the current through the MOSFET with R2. With the back-to-front Schottky clamping the output, the controller would keep increasing the current through the MOSFET to try and get the voltage up but there would be some limit to that, so the part's dissipation wouldn't necessarily have been enough to destroy it.

     

    So you might try just reworking the Schottky [if the Schottky SMD package is the type with fold-under legs, they're easy to get off even with a standard soldering iron as you can lift one end at a time]. Are you able to substitute a bench supply for the power rail? If so, one approach might be to apply a very low voltage that was under the controllers's lock-out voltage and was safe for the following circuit and see if the MOSFET feeds that to the coil without there being any gate drive.

     

    The feedback arrangement is a bit odd [and, possibly, a bit dangerous]. If you lost the connection to R6 you'd lose the feedback and the converter would ramp up the voltage to try and compensate, so you want to be careful with that depending on where it comes from and what it's supposed to be doing.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 7 years ago

    Resistance reading in-circuit is difficult because of paths round through the power and through the ICs [via the protection circuits]. You'll tend to see initially low readings that move because you're charging decoupling capacitors. I don't like doing it because of the possibility of damage to chips [a handheld meter is probably worse than a good bench meter in that respect], but then I tend to be very over-cautious.

     

    Commercially, you'd chuck the components and use new ones (the parts cost is much, much lower than the cost to you of a person messing around with parts that are suspect). Actually, you might well label the board carefully, put it to one side, and move to the next, unused prototype, unless there were good reasons for sticking with the same one.

     

    For a personal project it's different and you may want to experiment a bit. The MOSFET and Schottky are fairly robust. Just because you can't bear to touch it doesn't mean it is dead. The controller is working current mode, monitoring the current through the MOSFET with R2. With the back-to-front Schottky clamping the output, the controller would keep increasing the current through the MOSFET to try and get the voltage up but there would be some limit to that, so the part's dissipation wouldn't necessarily have been enough to destroy it.

     

    So you might try just reworking the Schottky [if the Schottky SMD package is the type with fold-under legs, they're easy to get off even with a standard soldering iron as you can lift one end at a time]. Are you able to substitute a bench supply for the power rail? If so, one approach might be to apply a very low voltage that was under the controllers's lock-out voltage and was safe for the following circuit and see if the MOSFET feeds that to the coil without there being any gate drive.

     

    The feedback arrangement is a bit odd [and, possibly, a bit dangerous]. If you lost the connection to R6 you'd lose the feedback and the converter would ramp up the voltage to try and compensate, so you want to be careful with that depending on where it comes from and what it's supposed to be doing.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I wasn't sure how possible it was to test in-circuit and how skewed the result would be. 

     

    However, having taken both pieces of the board, the Schottky rectifier is reading 0.159Ohms and OL; a known good one is reading 0.157Ohms and OL.  I think that's ok and I put it back on the board in the correct orientation.

     

    The Mosfet is reading 0.33Ohms between drain and source (out of circuit).  A known good one is reading >34MOhms.  So I think the one I removed is dead.  In goes a new one and back to testing.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer