Member's Forum Testing a Mosfet and Schottky in-circuit; Bit more advice
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 27 answers
  • Subscribers 630 subscribers
  • Views 8856 views
  • Users 0 members are here
Related

Testing a Mosfet and Schottky in-circuit; Bit more advice

Andrew J
Andrew J over 7 years ago

I presume this is possible with power off, looking for resistance between drain and source?

 

I'm pretty sure I've killed it - resistance is 0.33Ohms between these two pins image  Out of circuit, on a good one, it is > 13MOhms.  Looking at my circuit, I've solder the Schottky Rectifier the wrong way around - cathode to ground imageimageimage  Pretty sure that won't have done the Mosfet any good, it was too hot to touch.  Can't believe I've been so stupid - by good luck, rather than management, the other Schottky I have in the circuit (not shown below) is the right way around.

 

Is there a way of testing the Schottky rectifier in-circuit - I've tried it and the DMM 'beeps' as it detects a normal junction; measures 0.159v and 0.579V depending upon orientation of test leads?  Just to clarify - in the schematic below you can see how the Schottky rectifier should be - however, as I say, it's actually reversed and I don't know if that might affect readings. So, with the COM lead to the cathode and test (red) lead to anode it reads 0.159v; with the COM lead to the anode and test (red) lead to cathode it reads 0.579V.  I can test one out of circuit and I get 0.157V and OL respectively.  I think that indicates it is ok but in circuit it isn't reading as OL: I have to remove it to swap it around in any case so would the advice be to chuck it and use a new one? 

 

I'm really hoping I can get it off with wick and an iron and without damaging the board; ditto the Mosfet. I really don't want to lump out for a rework station.

 

Is there likely to be damage to other components down stream?  Any tips for testing components without removing them from the circuit?

 

This is only part of the circuit but shows the relationship between the Mosfet and Schottky rectifier:

 

image

 

[silently screaming inside]

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 7 years ago

    Hi Andrew,

     

    Try reading the diode with just a regular Ohm meter. You should see low ohms in one direction and very high ohms in the other. Your  0.579 V sounds a little too high for a schottky and the 0.159 volts sounds way too low. In circuit however can confuse the readings. Out of the circuit you should only get a voltage reading in one direction with the diode test.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to jw0752

    image

     

    0.159V doesn't look too unreasonable for a test current of between 1mA and 10mA.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I measured the current of the DMM in diode test mode and it generates 1mA so I thought it may be ok; the out-of-circuit reading for the other direction is OL rather than 0.579V so I may not be out of the woods.  However, doing a bit of reading around, I find that a reading of 0.5v to 0.8v could be expected.  The DMM is also beeping to indicate a normal junction rather than a short-circuit.  I have to take it out anyway so if I do and don’t read OL then I shall chuck it.

     

    I’ll also test the resistance as you say John and see what results.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I measured the current of the DMM in diode test mode and it generates 1mA so I thought it may be ok; the out-of-circuit reading for the other direction is OL rather than 0.579V so I may not be out of the woods.  However, doing a bit of reading around, I find that a reading of 0.5v to 0.8v could be expected.  The DMM is also beeping to indicate a normal junction rather than a short-circuit.  I have to take it out anyway so if I do and don’t read OL then I shall chuck it.

     

    I’ll also test the resistance as you say John and see what results.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer