Member's Forum Documentation of projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 10 answers
  • Subscribers 631 subscribers
  • Views 3511 views
  • Users 0 members are here
  • documentation
  • schematics
  • docs
  • learning
Related

Documentation of projects

brianchilders
brianchilders over 7 years ago

    What are some tools that you use to document projects?

 

For example, when I look at projects online, they often have a BOM (Bill of Materials) as well as pictures of the project.

 

But when it comes to documenting the actual schematics, this is an area where I see less of.  I understand that there may be varying levels of experience, but as I share my ideas here, I would like for others to easily build or reproduce what I've done.

 

In addition to technical schematics, is there a program that makes a "pretty picture" e.g. how parts might be laid out on a breadboard?

 

Thanks for your help!

 

-brian

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Brian,

     

    There's a few breadboard diagramming applications, I believe Fritzing will do it. For stripboard layouts (i.e. similar-ish to breadboard) I've use Lochmaster once, it is not free software, but as long as you're ok not saving your project, then you can use the free demo version and click the Print Screen button to copy the output to your clipboard, and then paste into MS Paint etc., to save it. It is ok-ish. I just used the free version, to me it wasn't worth the asking price because I rarely draw such diagrams (there's huge scope for errors if people rely on bradboard layouts alone, without knowing IC pin numbers etc., so at some point if they can, then they may as well start examining real schematics. But the schematic may not be enough, since interpreting a schematic is likely not possible for projects intended for children or beginners in electronics.

     

    PowerPoint is an option too. This diagram was done with it (showing connections between dev-boards for example):

    image

    I like using PowerPoint, but I appreciate it is an acquired taste. it is useful for block diagrams too, to help explain the circuit before showing the schematic.

    image

    If you're not into PP, then Visio is an alternative.

     

    Generally I'll just use a conventional schematic too (using EAGLE in my case, but there's plenty of options), and then try to have a detailed photo of the PCB or breadboard too.

    image

     

    EDIT: One more thing, personally I feel high-res helps for everything : ) That block diagram above was drawn six years ago, but since I'd saved it in a high-res, it still looks readable without needing to zoom in heavily, on the more modern super-high-res monitors, despite having drawn the diagram on probably a 1024x768 screen 6 years ago. Just personal taste has changed since then though.. now I'll often use a white background for such things, and thicker lines and a larger font. Not everyone likes large file sizes perhaps, but I have to make a compromise somewhere, and if I have to make that choice then it will be on the side of readability.

    It is really sad seeing valuable books and documents with diagrams that are low-res and unreadable, or hard to follow monochrome photos using halftone dots. I know that was the technology limit with printing at the time, but it is still sad, especially when it is an interesting piece of work and you know it would have been exciting to see the photo in slightly higher-res.

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi Brian,

     

    There's a few breadboard diagramming applications, I believe Fritzing will do it. For stripboard layouts (i.e. similar-ish to breadboard) I've use Lochmaster once, it is not free software, but as long as you're ok not saving your project, then you can use the free demo version and click the Print Screen button to copy the output to your clipboard, and then paste into MS Paint etc., to save it. It is ok-ish. I just used the free version, to me it wasn't worth the asking price because I rarely draw such diagrams (there's huge scope for errors if people rely on bradboard layouts alone, without knowing IC pin numbers etc., so at some point if they can, then they may as well start examining real schematics. But the schematic may not be enough, since interpreting a schematic is likely not possible for projects intended for children or beginners in electronics.

     

    PowerPoint is an option too. This diagram was done with it (showing connections between dev-boards for example):

    image

    I like using PowerPoint, but I appreciate it is an acquired taste. it is useful for block diagrams too, to help explain the circuit before showing the schematic.

    image

    If you're not into PP, then Visio is an alternative.

     

    Generally I'll just use a conventional schematic too (using EAGLE in my case, but there's plenty of options), and then try to have a detailed photo of the PCB or breadboard too.

    image

     

    EDIT: One more thing, personally I feel high-res helps for everything : ) That block diagram above was drawn six years ago, but since I'd saved it in a high-res, it still looks readable without needing to zoom in heavily, on the more modern super-high-res monitors, despite having drawn the diagram on probably a 1024x768 screen 6 years ago. Just personal taste has changed since then though.. now I'll often use a white background for such things, and thicker lines and a larger font. Not everyone likes large file sizes perhaps, but I have to make a compromise somewhere, and if I have to make that choice then it will be on the side of readability.

    It is really sad seeing valuable books and documents with diagrams that are low-res and unreadable, or hard to follow monochrome photos using halftone dots. I know that was the technology limit with printing at the time, but it is still sad, especially when it is an interesting piece of work and you know it would have been exciting to see the photo in slightly higher-res.

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer