Member's Forum Miniature, pleasent-sounding buzzer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 6 answers
  • Subscribers 632 subscribers
  • Views 3137 views
  • Users 0 members are here
  • buzzers
Related

Miniature, pleasent-sounding buzzer

StevenS
StevenS over 6 years ago

I have an Itaki cooking lunch box, which is a tiny Japanese 200W steamer, made to take your lunch to work and heat it.

 

Its operation is pretty simple: It has a heating element, switch, pilot light, and temperature-controlled switch. You put water it in, and when the water boils off, the temperature rises and turns the heating element off.

 

The trouble is that there is no audible alert when it is done - you have to set a timer and keep checking the pilot light.

 

I want to add a buzzer that will make sound when it's done cooking. My plan is to take the voltage that will be across the temperature-controlled switch. I'll have a capacitor in series to drop the voltage, and a full-wave rectifier to make DC to power a 5v or 12v buzzer.

 

My issue is that I'd like to use a buzzer that sounds pleasant, not annoying. A repeating "ding" would be nice, but I can't find anything to buy that sounds pleasant and will fit in the small space I have.

 

Do you know where I could buy such a sounder?

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 6 years ago

    Hi Steven,

     

    Your idea interested me so I breadboarded it on my bench. I used your description of a power circuit as shown in this schematic:

     

    image

    I found a small sonalert that sounds a lot like the steam whistle of an old fashion teapot. At 5 volts it drew 20 mA so using the Xc formula I calculated that I would need about 500 nF in series with the bridge rectifier in order to supply a comparable current from my 115 V 60 Hz line voltage. In the schematic above, the label on the capacitor should read 100 nF / 4 mA. You will have to measure the current draw at operational voltage for the sonalert that you choose. It might be best to choose one that has a steady sound as this circuit is designed assuming a pretty constant load and the circuit will attempt to deliver a current of 20 mA by increasing the voltage across the buzzer. If you do decide to use a sonalert that doesn't present a constant load to the line you could put a zener diode across the buzzer to keep the voltage from damaging it.

     

    The challenge will be to get all the components into a safe enclosure since you are dealing with line voltages and fatal shock hazards. Here is the result of my test circuit.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    I look forward to seeing your completed build.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jackng
    0 jackng over 5 years ago in reply to jw0752

    Hey John and Steven, I too am looking for a buzzer that's pleasant, for a fitness device. If anyone used a Philips Sonicare Toothbrush, it gives a very subtle and pleasant beep every 30 seconds. That's exactly the outcome I'm going for. I wonder if you need a circuit and resistor to attenuate the output, or some off the shelf component available?

    The common buzzers are designed to be loud, high pitch and annoying because that's their purpose, to alarm people. But Steven and I are looking for the opposite, to build an audio cue, that is pleasant.
    Cheers, Jack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jackng
    0 jackng over 5 years ago in reply to jw0752

    Hey John and Steven, I too am looking for a buzzer that's pleasant, for a fitness device. If anyone used a Philips Sonicare Toothbrush, it gives a very subtle and pleasant beep every 30 seconds. That's exactly the outcome I'm going for. I wonder if you need a circuit and resistor to attenuate the output, or some off the shelf component available?

    The common buzzers are designed to be loud, high pitch and annoying because that's their purpose, to alarm people. But Steven and I are looking for the opposite, to build an audio cue, that is pleasant.
    Cheers, Jack.