Products
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
Member's Forum Improving a Reflectance Sensor design for high speed reading
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 630 subscribers
  • Views 2974 views
  • Users 0 members are here
  • analog input
  • tachometer
  • encoder
  • comparator
  • lm393
  • ir sensor
  • analog
  • darlington pair
Related

Improving a Reflectance Sensor design for high speed reading

luislabmo
luislabmo over 6 years ago

I've been prototyping with a Reflectance Sensor to be used in different applications with a micro-controller, mostly as a speed sensor and as an encoder. My goal is to try to use it as best as I can at high speeds which at the end of the day is just reading Reflectance -or Not- for pulses that last a very short amount of time. Below is the Schematic in question - this design is not originally mine but seems to be the go-to design for many hobbyist IR Sensors.

image

First I tried working with just the circuit enclosed inside the Reflective Object Sensor area which produces an analog signal, but at high speeds the signal doesn't rise fast enough, with that in mind, leaving out the Comparator (LM393) or any solution that helps mitigate this problem is probably out of the question.

 

  1. Low Speed test: to my surprise, I noticed that the LED helps in the design image. It helps the signal rise faster or makes it look more like a square wave -which is a good thing as I'm reading the output using an external interrupt. I noticed when the LED (D1) is replaced with any diode, the output looks even better (on the downside it adds a ringing to the base voltage). Could someone explain why a Diode seems to help here? and why, as I increase the value of R5, the Base voltage tends to be lower? -again another good thing for the design seems. In this test I tried different diodes 1N5227B Zenner Diode1N5227B Zenner Diode, 1N914 Signal Diode1N914 Signal Diode and 1N4007 all with the same results.
    image
  2. High Speed test: It seems that the current value of C3 is too high and affects the output when the sensor is reading reflectance at high-speeds (the pulses don't rise high or fast enough for the micro-controller to read High). In that case, what could be a better trade off? - adding the Diode and/or lowering C3 to lets say 0.01µF.
    image
  3. Keeping the LED: adding the Diode seems to be a good approach -or maybe there is a different way-. What could be the best way of keeping the LED also? -It's a great way to have a visual feedback when the sensor is doing it's job and also to help calibrating the sensor.

 

If you made it this far, thank you for reading. Please let me know what you think in the comments.

 

Luis

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Luis!

     

    There's a few things to try:

    Firstly (very important) there needs to be a 100nF capacitor* directly across the supply rails of U1. You may already have done this (it's not on the circuit diagram).

    I sometimes wire it diagonally across the chip, to keep the leads short (example photo below of a different chip, but you can see how it is placed on top of the chip to keep the length as short as possible).

    Also, D1, R5 and C3 are not needed, if you're connecting to a microcontroller. However, try reducing R3 from 10k to (say) 1k to see if it improves things. The current consumption will increase, but this isn't so significant in this circuit because the LED in the reflectance device will be using more current anyway.

    Also, the datasheet suggests implementing hysteresis, as in figure 22 of the TI datasheet.

    Finally, if this is on breadboard, maybe shorter wires could help.

     

    * 100nF axial capacitors100nF axial capacitors are convenient for wiring across the chip, but really any 100nF capacitor will do.

     

    EDIT: Also, if there is an unused comparator in that chip as there seems to be from the schematic, then you can connect one input to ground (via say a 1k resistor) and another input to the supply (via another 1k resistor) so that no output circuitry for the unused comparator is (potentially) unstable.

     

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi Luis!

     

    There's a few things to try:

    Firstly (very important) there needs to be a 100nF capacitor* directly across the supply rails of U1. You may already have done this (it's not on the circuit diagram).

    I sometimes wire it diagonally across the chip, to keep the leads short (example photo below of a different chip, but you can see how it is placed on top of the chip to keep the length as short as possible).

    Also, D1, R5 and C3 are not needed, if you're connecting to a microcontroller. However, try reducing R3 from 10k to (say) 1k to see if it improves things. The current consumption will increase, but this isn't so significant in this circuit because the LED in the reflectance device will be using more current anyway.

    Also, the datasheet suggests implementing hysteresis, as in figure 22 of the TI datasheet.

    Finally, if this is on breadboard, maybe shorter wires could help.

     

    * 100nF axial capacitors100nF axial capacitors are convenient for wiring across the chip, but really any 100nF capacitor will do.

     

    EDIT: Also, if there is an unused comparator in that chip as there seems to be from the schematic, then you can connect one input to ground (via say a 1k resistor) and another input to the supply (via another 1k resistor) so that no output circuitry for the unused comparator is (potentially) unstable.

     

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • luislabmo
    0 luislabmo over 6 years ago in reply to shabaz

    Hi Shabaz!.

     

    You guessed well, I'm using a breadboard and that's one the reasons there is considerable noise in the screen captures -actually is my first time ever with an analog circuit and using a comparator, naturally I didn't feel comfortable going directly to a PCB design without trying it first with a spiderweb of wires.

     

    I removed the components you suggested and added the hysteresis, the signal changes real fast... nice catch from your side, Thank you!  -Still trying to understand the formulas as seems hysteresis in my case only works when the resistor in series with the input is added (red arrow in the diagram)

    image

    Let me ask one more. I'm planning -hopefully- to use the sensor in some noisy environments with motors and maybe some long wires (2 or 3 feet long). Is it better practice to include the sensor and the comparator close the motor (sending the comparator's output through the wires) or should I keep the comparator closer to the micro-controller? in which case the IR sensor output would be the one traveling through the wires.

     

    Luis