• Products and Partners
    Products and Partners
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
Member's Forum Cutting power to a circuit by time elapsed.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 8 answers
  • Subscribers 631 subscribers
  • Views 1995 views
  • Users 0 members are here
Related

Cutting power to a circuit by time elapsed.

cookekeyes
cookekeyes over 6 years ago

I had an idea the other day and I wanted to ask about the specifics of it here.

 

So, I have a few guitars that use active pickups, meaning they require batteries (usually 9v) and one annoying aspect of them is if you leave a cable plugged into the guitar’s output jack, it’ll continue to drain the battery. Normally this isn’t a huge issue, but there are times when I forget to unplug it or I leave it plugged in for a few hours when I go to do something else.


Anyway, I thought it would be cool if I could add a circuit that could cut the power based on how much time has elapsed without a signal. It would need to be fairly small, as it needs to fit in the guitar’s control cavity and preferably be independent of any of the guitar’s circuitry. I don’t want the signal chain going through anything that could affect the tone. You’d think manufacturers would include something like this already, and maybe they do, but the 3 guitars I have with active pickups don’t have it.

Since I’m a complete novice when it comes to designing circuits, I thought I’d ask here. The only thing I could think of was maybe a 555 timer, but I know next to nothing about them. I remember Ben did something similar on an old episode with a baby monitor and music player, but he used a lot of the existing circuitry from the monitor if I recall correctly.

 

Well, that’s my idea. Thanks for any help or advice.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    Almost certainly best to base it on a tiny processor. There will have be some connection to the guitar to check the signal. I recently used some of these for an emergency patch -

     

    STM32G031J6M6, ARM processor with ADC in 8 pin SOIC package - can run at 2MHz clock and use about 0.2mA - which I guess will be a lot less than the normal operating current.

     

    Once the power has gone off the processor can sleep and draw less than 1uA (battery run down in 500,000 hours) - other bits may use more power !

     

    You could use a TI TPS22810 for the power switch. You'll also need a micropower regulator for the processor.

     

    I've attached a picture of my STM32G031J6M6 application to give you an idea of achievable size:

     

    image

     

    I'm not offering to design this for you - I have time to help a bit but not to do it all, it would be an ambitious project for a novice - you might be able to team up with some other people.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 6 years ago

    Almost certainly best to base it on a tiny processor. There will have be some connection to the guitar to check the signal. I recently used some of these for an emergency patch -

     

    STM32G031J6M6, ARM processor with ADC in 8 pin SOIC package - can run at 2MHz clock and use about 0.2mA - which I guess will be a lot less than the normal operating current.

     

    Once the power has gone off the processor can sleep and draw less than 1uA (battery run down in 500,000 hours) - other bits may use more power !

     

    You could use a TI TPS22810 for the power switch. You'll also need a micropower regulator for the processor.

     

    I've attached a picture of my STM32G031J6M6 application to give you an idea of achievable size:

     

    image

     

    I'm not offering to design this for you - I have time to help a bit but not to do it all, it would be an ambitious project for a novice - you might be able to team up with some other people.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer