• Products and Partners
    Products and Partners
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
Member's Forum Cutting power to a circuit by time elapsed.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 8 answers
  • Subscribers 631 subscribers
  • Views 1995 views
  • Users 0 members are here
Related

Cutting power to a circuit by time elapsed.

cookekeyes
cookekeyes over 6 years ago

I had an idea the other day and I wanted to ask about the specifics of it here.

 

So, I have a few guitars that use active pickups, meaning they require batteries (usually 9v) and one annoying aspect of them is if you leave a cable plugged into the guitar’s output jack, it’ll continue to drain the battery. Normally this isn’t a huge issue, but there are times when I forget to unplug it or I leave it plugged in for a few hours when I go to do something else.


Anyway, I thought it would be cool if I could add a circuit that could cut the power based on how much time has elapsed without a signal. It would need to be fairly small, as it needs to fit in the guitar’s control cavity and preferably be independent of any of the guitar’s circuitry. I don’t want the signal chain going through anything that could affect the tone. You’d think manufacturers would include something like this already, and maybe they do, but the 3 guitars I have with active pickups don’t have it.

Since I’m a complete novice when it comes to designing circuits, I thought I’d ask here. The only thing I could think of was maybe a 555 timer, but I know next to nothing about them. I remember Ben did something similar on an old episode with a baby monitor and music player, but he used a lot of the existing circuitry from the monitor if I recall correctly.

 

Well, that’s my idea. Thanks for any help or advice.

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 6 years ago

    Hello, frankly I think the MK is correct to make something nice and smart but – if I have understood – you are searching for help or advice that gives you the possibility to manage and control by yourself the building, not a sort of specific product well done by just plug and play.

    If I am not wrong, can you tell a bit more how and when the circuit power should but cut? when there are no signals on the cable? maybe that with something simpler it is possible to solve the problem. Or not, but at the moment I have not sufficient information.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 6 years ago

    Hello, frankly I think the MK is correct to make something nice and smart but – if I have understood – you are searching for help or advice that gives you the possibility to manage and control by yourself the building, not a sort of specific product well done by just plug and play.

    If I am not wrong, can you tell a bit more how and when the circuit power should but cut? when there are no signals on the cable? maybe that with something simpler it is possible to solve the problem. Or not, but at the moment I have not sufficient information.