• Products and Partners
    Products and Partners
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
Member's Forum Member Generated Stepper Motor Pinout Quiz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 630 subscribers
  • Views 823 views
  • Users 0 members are here
  • stepper motor quiz
Related

Member Generated Stepper Motor Pinout Quiz

colporteur
colporteur over 6 years ago

image

Assign the labels (A+, A-, B+, B- ) to the pins (w,x,y,z) on the motor windings and to the columns (C1, C2, C3, C4) of the table, that will enable the shaft to rotate in the clockwise direction. The sequence that the voltage is applied to the motor pins is shown in the table.

 

Your answer should be in the form w=A+...z=B-  & C1=A+….C4=B-. No these examples are not the start of the answer.

 

I suspect I have incorrect manufacture documentation. The documentation indicates the step sequence for the stepper motor will rotate the shaft clockwise. The stepper motor does rotate in a clockwise direction with the sequence provided but stepper motor theory would suggest otherwise. 

 

I have exhausted my stepper motor knowledge to make sense of the vendor drawings. If I use the motor pinout and winding diagram from the documentation with my understanding of motors the shaft should rotate anticlockwise with the sequence provided. I have used my theory knowledge to test against other vendors motors and it appears correct. When I make one pinout change on the vendors drawing the sequence and the rotation match motor theory.

 

I have a personally that can't ignore such a conflict. WHO CARES IT WORKS! I wish at times, I was one of those people. I have worked this problem off and on for a few days and can’t seem to resolve the conflict. My solution, create a discussion quiz and see what the E14 Community members can provide. I'm hoping your answers will match my understanding:)

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 6 years ago

    Is it possible they are looking at the motor from the opposite direction that you are?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 6 years ago in reply to dougw

    The specification documentation show the front of the motor, the connector and the pinout.

     

    I plugged the motor into an A4988 driver and the output sequenced worked in the correct direction. The issue is at the schematic of the motor itself. If I use the pinout provided the motor is anticlockwise. If I reverse the pins on one winding and the theory worked.

     

    I'm hoping someone with more motor experience than me looks at the drawing and just knows from experience the order for the pins.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 6 years ago in reply to dougw

    The specification documentation show the front of the motor, the connector and the pinout.

     

    I plugged the motor into an A4988 driver and the output sequenced worked in the correct direction. The issue is at the schematic of the motor itself. If I use the pinout provided the motor is anticlockwise. If I reverse the pins on one winding and the theory worked.

     

    I'm hoping someone with more motor experience than me looks at the drawing and just knows from experience the order for the pins.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer