• Products and Partners
    Products and Partners
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
Member's Forum Suggestions for C Language IDE?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 12 answers
  • Subscribers 635 subscribers
  • Views 3457 views
  • Users 0 members are here
  • c language
  • visual studio 2019
  • eclipse ide
  • c-c++ programming
  • c code
  • c programing language
Related

Suggestions for C Language IDE?

mudz
mudz over 5 years ago

Which IDE you use or have used for C programming? Which one you like the most and why?

/﹋\

(҂`_´)

<,︻╦╤─ ҉      c c c c c c c c c c c c c   ▬▬▬.◙.▬▬▬

  /﹋\                                                     ═▂▄▄▓▄▄▂

                                                            ◢◤ █▀▀████▄▄▄▄◢◤

                                                            █▄ █ █▄ ███▀▀▀▀▀▀▀╬

                                                            ◥█████◤

                                                            ══╩══╩═

 

Update ------

Spent a lot of time on eclipse but wasn't able to get it in working mode, Tried Visual studio again and it worked just needed a little bit of tinkering. it worked but output .exe false detected by Bitdefender antivirus and got quarantined automatically. Added folder to exceptions. Hmmm, may be VS not that bad ! Lets c how it goes.
Will definitely keep working on eclipse, will learn things doing so.

I'll keep on updating !!
Thank you all 
image

 

p.s- This discussion isn't over yet, all suggestions are most welcome.

 

Message was edited by: mudz

 

Update 2 ------

Interestingly I did something, and it worked. So, eclipse is working as well for now. I've no idea. Cygwin64 to mingw.. ¯\_(ツ)_/¯

 

Message was edited by: mudz

  • Sign in to reply
  • Cancel
  • mrmnt63
    0 mrmnt63 over 5 years ago

    As a free simple editor, I like Notepad++. It supports many languages in one place with highlighting and syntax help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mrmnt63
    0 mrmnt63 over 5 years ago in reply to mudz

    Sololearn.com is a helpful re-introduction to get you back into the swing. It has many languages and is a great introduction if you want to try to learn something from scratch as well. It has quizzes and examples. Allows for saving code you write and allows you to modify and play around with the example code it provides. It is set up so you can do a few minutes at a time and pick-up where you left off. It covers all the important stuff at a minimal level of depth. It is an easy starting point.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 5 years ago

    You might like Pelles C,

     

    smorgasbordet - Pelles C

     

    Much smaller and more plain simple C than most. ABout as near to Turbo C as you 'll get on a modern PC.

     

    And free.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 5 years ago

    I am going to suggest Segger Embedded Studio. Oddly this is one IDE I know the least about and yet I have found it to be one of the better ones to use. The reason I got to use it was through a Taiyo Yuden BLE module and a Panasonic BLE module road test. It just does the job and so I find myself going back to it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • koudelad
    0 koudelad over 5 years ago

    I could recommend Atom and Visual Studio Code as free and CLion as a paid, full-featured IDE.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 5 years ago

    What OS are you working with?

     

    On Linux, for just simple C development, either vi or vim.  With vim you can add features where you can do syntax highlighting and such.

    For IDE specific, Eclipse would be the first one.

    Code::Blocks is another one which is cross platform: Windows, Linux, Mac OS X, Raspberry Pi.

    Visual Studio Code as an Editor with compile done via command line but working on using it as a compiler.

    Atom is another simple editor.

     

    Windows: Eclipse, Visual Studio, Visual Studio Code pretty much in that order.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 5 years ago

    Just wrote about my latest favorite semi-colon language for PC to learn programming:

     

    Hidden Gem:  The "Processing IDE" for... | element14 | Arduino Projects

     

    Not exactly C, but very similar and translates to microcontrollers well down the road.

     

    -Sean

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to mudz

    mudz  wrote:

    ...

    image

     

    Try out C++20 Preview: set up a development environment

    If you think you've set up your toolchain correctly already at the moment, try this: Project -> Properties -> C / C++ Build -> Builder Type -> Internal Builder.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago

    Exactly as Fred and Jan say.. for coding for Windows targets, why not use Visual Studio, it is already tightly integrated and ready to use, plus there will be plenty of examples online. It's not 'too complex' - just takes a bit of effort to find a tutorial that you're comfortable with. There's thousands of books on Windows programming, they almost all use Visual Studio.

     

    If you're just beginning to learn C without making use of any Windows libraries and perhaps just standard input/output to the terminal, then is an IDE needed? People write programs (even huge ones) without an IDE too. They just use the code editor of their choice, and do the build using scripts. You'll need to learn how to use makefiles anyway, what better way than to learn to do it for a simple C program.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mudz
    0 mudz over 5 years ago in reply to Fred27

    For simple C programming learning not for any hardware device like microcontroller/processor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>