Member's Forum Searching for specific flat flexible cable, not easy task :-(
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 3386 views
  • Users 0 members are here
Related

Searching for specific flat flexible cable, not easy task :-(

dogrox
dogrox over 12 years ago

Hello I'm new to this forum so bear with me if I'm not in the right area posting this question.  I've been searching for a specific flat flexible cable that I didn't realize was going to be this complicated to find. I'm working on my Korg keyboard. I need flexible cable for a modified floppy drive adapter I'm installing. I've had no luck searching for one anywhere, and believe me I've looked everywhere. The specs I need are:

 

24 pin

1.25mm pitch

Contacts Opposite Sides of each other.

At least 14 inches long, no less.

 

I have checked this one site where I'm logged in at where I get quotes from different companies but it seems like they want a minimum order for a thousand cables match is way too many all I need is a few. Why are these cables so hard to find?

 

If anybody has any advice where I can pick up a few of these csbles like this I'd appreciate it ...thanks!,

 

Dog

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    Are you looking for a ribbon cable assembly with a connector on it?

    Normally cable with this pitch is single-sided "flex" - the wires are just traces on a flexible substrate and the "connector" is just the bared ends of the traces (which are plated to minimize oxidation) - they just get clamped into a pcb-mounted flex connector. The connector pins may be separated into 2 rows for connection to the PCB, but internally the cable connections are on only one side of the cable...

    Flex cable is almost always custom made for a specific application because the "connectors" are plated, making it unsuitable for trimming to size - consequently there are only a few "standard" high-volume sizes on the market.

    Do you have a picture or a sketch of what you are looking for?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago

    Are you looking for a ribbon cable assembly with a connector on it?

    Normally cable with this pitch is single-sided "flex" - the wires are just traces on a flexible substrate and the "connector" is just the bared ends of the traces (which are plated to minimize oxidation) - they just get clamped into a pcb-mounted flex connector. The connector pins may be separated into 2 rows for connection to the PCB, but internally the cable connections are on only one side of the cable...

    Flex cable is almost always custom made for a specific application because the "connectors" are plated, making it unsuitable for trimming to size - consequently there are only a few "standard" high-volume sizes on the market.

    Do you have a picture or a sketch of what you are looking for?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dogrox
    0 dogrox over 12 years ago in reply to dougw

    Thank you for responding. I am aware of the specifications of flat fexible cable. I do not need the connectors themselves as they are on the pcbs.  I do not have drawings nor images of the cables i need. All I can provide is what specs I provided in my original post. I figured that the people that sell the cables would know what I needed by the specs I provided.  Thank you again.