Member's Forum Searching for specific flat flexible cable, not easy task :-(
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 3400 views
  • Users 0 members are here
Related

Searching for specific flat flexible cable, not easy task :-(

dogrox
dogrox over 12 years ago

Hello I'm new to this forum so bear with me if I'm not in the right area posting this question.  I've been searching for a specific flat flexible cable that I didn't realize was going to be this complicated to find. I'm working on my Korg keyboard. I need flexible cable for a modified floppy drive adapter I'm installing. I've had no luck searching for one anywhere, and believe me I've looked everywhere. The specs I need are:

 

24 pin

1.25mm pitch

Contacts Opposite Sides of each other.

At least 14 inches long, no less.

 

I have checked this one site where I'm logged in at where I get quotes from different companies but it seems like they want a minimum order for a thousand cables match is way too many all I need is a few. Why are these cables so hard to find?

 

If anybody has any advice where I can pick up a few of these csbles like this I'd appreciate it ...thanks!,

 

Dog

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 12 years ago

    Hi there a picture of the cable if it's still about will help failing that a picture of the two ends so folk can guess the connector type.

    The 1.25mm pitch is just standard since that's what is used to connect to 2 rows of .1" pitch connector.

     

    Normally you'd be looking at some 26way ribbon and two IDC connectors so to be more accurate you may be best to take that photo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 12 years ago

    Hi there a picture of the cable if it's still about will help failing that a picture of the two ends so folk can guess the connector type.

    The 1.25mm pitch is just standard since that's what is used to connect to 2 rows of .1" pitch connector.

     

    Normally you'd be looking at some 26way ribbon and two IDC connectors so to be more accurate you may be best to take that photo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 12 years ago in reply to Problemchild

    Butch, with that FPC you quite often find that the cable is in fact the same way round but it has a fold made in to it to rotate it. Might be worth a check .....half of those connections are probably ground so you can meter them to see which is which!