• Products and Partners
    Products and Partners
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
Member's Forum NooElec R820T SDR & DVB-T software setup procedures and first time user suggestions?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 631 subscribers
  • Views 3470 views
  • Users 0 members are here
  • new_member_introduction
Related

NooElec R820T SDR & DVB-T software setup procedures and first time user suggestions?

markacarter
markacarter over 11 years ago

     Dear sirs and mams.

Does anyone have any suggestions for the NooElec R820T SDR & DVB-T software setup procedures for the first time user?

My call sign is KD7PHW extra class.

 

     I am new to the Element 14 user community.

 

                                                                           Thank you.

 

                                                                         Mark A Carter

  • Sign in to reply
  • Cancel
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to hbb360

    If running on Windows, you will need to have the Realtek drivers installed (not Zadig/Libusb.org). Then any BDA compatible tuning software can be used - for example VLC (using the Open Capture Device option and configuring appropriately), ProgDVB (using the BDA input filter), AltDVB, DVB Dream, etc.

     

    If running on Linux, ensure that a V4L2 driver is available and the rtl283x kernel module is installed. Then you can use VLC, mumudvb, dvblast, etc as the tuning software.

     

    As far as I know, originally these types of dongles shipped with either BlazeVideo, MagicPVR, or Arcsoft Total Media Theatre depending on the OEM.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hbb360
    0 hbb360 over 8 years ago in reply to Gough Lui

    Hello everyone. I also have this dongle and would like to watch DVB-T TV with it but I can't seem to find any software that works with it... Could anyone link me to a piece of software that is compatible and would let me watch TV with this dongle?

    Thanks!

    Nik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 11 years ago

    Hi Mark,

     

    What do you want to do with it? Do you want to use it as an SDR radio receiver? If so, I suggest getting started with SDRSharp (SDR#). See some instructions http://rtlsdr.org/softwarewindows

     

    Otherwise, you might be interested in decoding aircraft positions and plotting them - in which case, check out ADSB# (or rtl1090, or dump1090 for linux users) and ADSBScope (ADS-B with RTL-2832 based USB TV dongles made easy! | Gough's Tech Zone)

     

    Maybe you want to watch TV? Well if you're in America, you're out of luck because the tuner doesn't support ATSC digital used in the US. But if you're in a DVB-T country, you can use the software on the provided CD, or you can try using other DVB tuning software like ProgDVB.

     

    I've done some random testing and experimenting with RTL2832 Tuners, rtl2832 | Gough's Tech Zone, but you might be able to find some things to do with it on rtl-sdr.com

     

    - Gough