Member's Forum SDIP IC to DIP conversion
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 628 subscribers
  • Views 6473 views
  • Users 0 members are here
  • dip
  • sdip
  • convert
  • dip_adapter
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

SDIP IC to DIP conversion

e14 Contributor
e14 Contributor over 11 years ago

Hi Everyone (potential experts and kind advice givers),

 

Recently I started an 8-bit computer home-brew project based on the 64 pin SDIP version of the Z80180. Which I didn't think of at ordering is that the CPU isn't going to fit any of my proto boards which are all DIP based. Naively I thought that shouldn't be much of a problem I'll just get a converter board from Element14, since then I discovered that isn't that easy (or I'm searching for the wrong thing). In any case I'm completely stuck on this, I've ordered a ROTH ELEKTRONIK IC adapter but it turned out to be the wrong one. I'd really like to use the 64 pin Z80180 CPU as it has a lot of things build in that I won't have to think about with the 40 pin version Z80.

 

Any advice would really be appreciated, I know there are some shops in the US that make these boards but the problem is I'm located in Europe.

 

Things I'm thinking about:

1. Do I need to design a board myself in Eagle and have it printed?

2. Get a whole bunch of wires and solder 64 SDIP socket to two sets of 32 pin DIP headers (something I'm not really looking forward to)

 

Thanks,

Thomas

  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    First off this is what you have? http://www.cpu-world.com/CPUs/Z180/Zilog-Z8018006PEC.html

    Zilog Z8018006PEC

     

    https://www.youtube.com/embed/QbCGhkbKLBY     Looks like a breadboard should work and this guy did a clean job of it. What do you think?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Thanks Clem on getting back. What I have is actually this: http://nl.rs-online.com/web/p/microprocessors/6259062/ which is advertised as PDIP but it's actually SPDIP (so it's advertised wrong). I'd more more then willing to just reorder the same in a dip packages. It's not like it's that expensive.

     

    They guy on the video clearly has a DIP version so they should be out there. Funny enough I have the same breadboard on which it doesn't fit

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    If you want to try for another one , see http://www.findchips.com/search/Z8018010PSG

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    If you want to try for another one , see http://www.findchips.com/search/Z8018010PSG

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Sorry could not find a successful answer.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Thanks for the help Clem. I've looked into the options you send but no company seems to be able to give me a straight answer. I decided to abandon the z80180 SDIP package and wait until element14 has the normal z80 in stock again it just means I have to build more logic in order to get a UART going. It's a shame to trash it, it seemed like the ideal package :-) Lesson learned, stay far away from SDIP