Member's Forum SDIP IC to DIP conversion
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 628 subscribers
  • Views 6473 views
  • Users 0 members are here
  • dip
  • sdip
  • convert
  • dip_adapter
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

SDIP IC to DIP conversion

e14 Contributor
e14 Contributor over 11 years ago

Hi Everyone (potential experts and kind advice givers),

 

Recently I started an 8-bit computer home-brew project based on the 64 pin SDIP version of the Z80180. Which I didn't think of at ordering is that the CPU isn't going to fit any of my proto boards which are all DIP based. Naively I thought that shouldn't be much of a problem I'll just get a converter board from Element14, since then I discovered that isn't that easy (or I'm searching for the wrong thing). In any case I'm completely stuck on this, I've ordered a ROTH ELEKTRONIK IC adapter but it turned out to be the wrong one. I'd really like to use the 64 pin Z80180 CPU as it has a lot of things build in that I won't have to think about with the 40 pin version Z80.

 

Any advice would really be appreciated, I know there are some shops in the US that make these boards but the problem is I'm located in Europe.

 

Things I'm thinking about:

1. Do I need to design a board myself in Eagle and have it printed?

2. Get a whole bunch of wires and solder 64 SDIP socket to two sets of 32 pin DIP headers (something I'm not really looking forward to)

 

Thanks,

Thomas

  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Found up to 56 sdip to dip but too expensive http://www.epboard.com/eproducts/ezadapter.htm#Shrink DIP (SDIP) to DIP Adapter. BTW, al the diferent types which are many: https://en.wikipedia.org/wiki/List_of_integrated_circuit_packaging_types

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem,

     

    Believe it or not but I found the answer and, believe it or not, it's actually simpeler than I thought. See the image....
    image

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    That is very innovative.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    That is very innovative.

    Clem