• Products and Partners
    Products and Partners
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
Member's Forum Hello, new here with a question regarding Lpad resistors.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 7 answers
  • Subscribers 631 subscribers
  • Views 4530 views
  • Users 0 members are here
  • lpad
  • Speakers
Related

Hello, new here with a question regarding Lpad resistors.

mrsouth
mrsouth over 5 years ago

First of I'm new so Hi, 

     I have been messing about with Lpads (I have a few horns I need to tame in P.A enclosures).  I have created a crossover in LTspice, added the appropriate Lpad resistor values then I ran a simulation to check everything over.  First the voltage supply was set to 56V (level required to drive 8 ohm speakers to their rated 400Watts) and set it as a sine wave at 8Khz.  The crossover and Lpad are definitely working as designed (tested with pink noise source and checked fourier as well), however the the first Resistor in the Lpad (R1) is dissipating 120Watts.    Which seems at odds with the 30Watt resistors I've seen in similar rated speaker cabs.  Our overlord google.com has told me they don't need to be high wattage resistors,  but the circuit and simulation here (designed using commonly available calculators) tells me otherwise.

 

 

image

R1 and R2 are the Lpad, R3 is the horn.

The rest being a 4th order for the horn and 2nd order for the woofer.

 

Any Ideas what I am doing wrong?

 

 

Many thanks.

 

P.S still trying to work out how this site all works, forgive me if I've posted in the wrong group or something.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Matthew,

     

    I didn't have a chance to read/examine this in detail, but what stuck out was that you simulated with a sine wave. That may explain why the real-life resistors are of a lower power rating, since ordinarily the average power from speech or music will be a lot less than the peak. Most resistors can easily withstand higher power provided it is not sustained for a long time.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to shabaz

    Good point Shabaz - in real full range prgramme material the amount of energy at high frequencies will only be a small proprtion of the total.

     

    @ mrsouth Looking at the circuit, at high frequencies we can approximate that the inductors are infinite impedance (open circuit) and the capacitors zero impedance (short cicruit).

     

    The horn driving arm of the filter becomes:

     

    image

     

    And half the delivered power will go into R1 and a quarter into each of R2 and R3.

    (remember this is an approximation !)

    So your results look sensible.

     

    How much power goes into R1 if you use noise rather than a sine wave excitation ?

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to shabaz

    Good point Shabaz - in real full range prgramme material the amount of energy at high frequencies will only be a small proprtion of the total.

     

    @ mrsouth Looking at the circuit, at high frequencies we can approximate that the inductors are infinite impedance (open circuit) and the capacitors zero impedance (short cicruit).

     

    The horn driving arm of the filter becomes:

     

    image

     

    And half the delivered power will go into R1 and a quarter into each of R2 and R3.

    (remember this is an approximation !)

    So your results look sensible.

     

    How much power goes into R1 if you use noise rather than a sine wave excitation ?

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • mrsouth
    0 mrsouth over 4 years ago in reply to kkazem

    Cheers for chiming in kkazem.  I have taken the advice of active crossovers for my other speakers, however this one is powered by a single mixer/amp and needs to be a super simple/portable unit so bi amping is not an option.  Since starting this thread I have pulled apart a set of wharfedale PA drivers of similar size and found the crossover they designed to be even more perplexing than mine.   Although I haven't started yet (project had to go on the back burner) I am going to build the circuit below as altered by Michael Kellett, and give it thorough testing before making the second one.   If it turns out to be too problematic then I will likely replace the compression drivers with something less aggressive wh9ich should mean less issues with Lpad design.  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kkazem
    0 kkazem over 4 years ago in reply to michaelkellett

    With a 4 ohm series resistor and the 8 || 8-ohm = 4 ohm load, they form a voltage divider of 4/8 = 0.50 or 50% of the input maximum gets to the output. This means you lose half of your amplifier's output in R1. That's not a great design. There are better ways of designing low pass and high pass, passive filters that avoid high losses like this. A better way is to Bi-amp your amplifier by using two smaller amps that each have an active filter between the pre-amp and the power amp so that you avoid high losses in the filtering and virtually 100% of your amp's power goes to the load.