Member's Forum Hello, new here with a question regarding Lpad resistors.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 7 answers
  • Subscribers 631 subscribers
  • Views 4495 views
  • Users 0 members are here
  • lpad
  • Speakers
Related

Hello, new here with a question regarding Lpad resistors.

mrsouth
mrsouth over 4 years ago

First of I'm new so Hi, 

     I have been messing about with Lpads (I have a few horns I need to tame in P.A enclosures).  I have created a crossover in LTspice, added the appropriate Lpad resistor values then I ran a simulation to check everything over.  First the voltage supply was set to 56V (level required to drive 8 ohm speakers to their rated 400Watts) and set it as a sine wave at 8Khz.  The crossover and Lpad are definitely working as designed (tested with pink noise source and checked fourier as well), however the the first Resistor in the Lpad (R1) is dissipating 120Watts.    Which seems at odds with the 30Watt resistors I've seen in similar rated speaker cabs.  Our overlord google.com has told me they don't need to be high wattage resistors,  but the circuit and simulation here (designed using commonly available calculators) tells me otherwise.

 

 

image

R1 and R2 are the Lpad, R3 is the horn.

The rest being a 4th order for the horn and 2nd order for the woofer.

 

Any Ideas what I am doing wrong?

 

 

Many thanks.

 

P.S still trying to work out how this site all works, forgive me if I've posted in the wrong group or something.

  • Sign in to reply
  • Cancel
Parents
  • mrsouth
    0 mrsouth over 4 years ago

    Thanks Guys,  I haven't worked out how to create a noise source higher than 1v p-p (using pink noise wave file for the V source).   I'll do that and get back.

     

     

    EDIT: O.K, I'm having trouble creating a 56V noise source.  Any Ideas?

    MS

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 4 years ago in reply to mrsouth

    Can you make it a 5.6 V or a 0.56 volt one. I believe the equations are linear and all you will have to do is multiply by the appropriate factor.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mrsouth
    0 mrsouth over 4 years ago in reply to jw0752

    I might have to do that,  I did manage to make a random voltage source at 56V, however when I dropped it into the circuit it was taking 10+sec to simulate 100nS of run time.  It was going to take days and I don't think that is quite right.

     

    I ran it again with pink noise at 1V. It measured 25mA going to the high pass, 25mA going to the low pass side (strange that it was exactly the same) and the same 25mA from the source.  I have definitely done something wrong with LTspice.

     

    Thanks for the suggestions.

     

    MS

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mrsouth
    0 mrsouth over 4 years ago in reply to michaelkellett

    Here it is, I have also attached the pink noise file I am using.

     

    Thank you for looking at this.

    Attachments:
    first crossover.asc.zip
    Play this audio clip
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mrsouth
    0 mrsouth over 4 years ago in reply to michaelkellett

    Here it is, I have also attached the pink noise file I am using.

     

    Thank you for looking at this.

    Attachments:
    first crossover.asc.zip
    Play this audio clip