• Products and Partners
    Products and Partners
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
Member's Forum Case to Case Connections
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 630 subscribers
  • Views 3202 views
  • Users 0 members are here
Related

Case to Case Connections

Andrew J
Andrew J over 5 years ago

I'm looking for ideas for connecting encased devices.  So PCB -> Panel <-air gap-> Panel -> PCB.  Better:  Free end (for crimping connector) -> Panel <-air gap-> Panel -> Free end (for crimping connector).  I'm just looking to transfer signals and low-current, low-voltage power in a cheap way.  Although PCB edge-mounted connectors are an available option, I can't use these.

 

An example solution would be an IDC connector with flat cable: flexible with a variety of potential contacts and easily obtained with pre-made cables.  It's easy to find PCB mounts and male/female connectors but a panel mount socket (or plug) seems non-existent.   

 

An alternative would be d-sub connectors.  Again, variety of potential contacts, easy to solder up, but quite large.  Easy to find male/female connectors as well as panel mount.  Cheap as chips, but quite large.

I've come across pluggable terminal blocks but these are expensive.

 

The hardest element to find seems to be the panel mount socket (except for d-sub) but I'm not sure that I'm searching with the right keywords.  It's even harder to find a panel mount socket that is not expensive.  I'd settle for d-sub but thought I'd throw this out there for ideas.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Andrew,

     

    'Modular' (RJ45) could be an option, since circular panel mount sockets are available, and the circular hole is easier to make than rectangular. Wiring them is simple/cheap, provided you're ok with twisted pairs. I've used RJ45 on a few projects, and I like it because I can use standard ready-made network cables. It might be too bulky though if you wanted something smaller. For higher density, maybe 'MDR' connectors? They were used for old SCSI connections, and are available in (say) 20-pin and 30-pin, and the connectors are panel mount usually.

    Regarding IDC connectors, there are some that are panel mount but they are more rare. This one maybe:

    https://uk.farnell.com/3m/4620-6000/header-idc-lugged-20way/dp/469166

    (It is panel mount but would use ribbon cable, to the PCB, or strip the other end of the ribbon cable and solder to the PCB or whatever).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago

    Hi Andrew,

     

    'Modular' (RJ45) could be an option, since circular panel mount sockets are available, and the circular hole is easier to make than rectangular. Wiring them is simple/cheap, provided you're ok with twisted pairs. I've used RJ45 on a few projects, and I like it because I can use standard ready-made network cables. It might be too bulky though if you wanted something smaller. For higher density, maybe 'MDR' connectors? They were used for old SCSI connections, and are available in (say) 20-pin and 30-pin, and the connectors are panel mount usually.

    Regarding IDC connectors, there are some that are panel mount but they are more rare. This one maybe:

    https://uk.farnell.com/3m/4620-6000/header-idc-lugged-20way/dp/469166

    (It is panel mount but would use ribbon cable, to the PCB, or strip the other end of the ribbon cable and solder to the PCB or whatever).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer