• Products and Partners
    Products and Partners
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
Member's Forum Case to Case Connections
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 630 subscribers
  • Views 3186 views
  • Users 0 members are here
Related

Case to Case Connections

Andrew J
Andrew J over 5 years ago

I'm looking for ideas for connecting encased devices.  So PCB -> Panel <-air gap-> Panel -> PCB.  Better:  Free end (for crimping connector) -> Panel <-air gap-> Panel -> Free end (for crimping connector).  I'm just looking to transfer signals and low-current, low-voltage power in a cheap way.  Although PCB edge-mounted connectors are an available option, I can't use these.

 

An example solution would be an IDC connector with flat cable: flexible with a variety of potential contacts and easily obtained with pre-made cables.  It's easy to find PCB mounts and male/female connectors but a panel mount socket (or plug) seems non-existent.   

 

An alternative would be d-sub connectors.  Again, variety of potential contacts, easy to solder up, but quite large.  Easy to find male/female connectors as well as panel mount.  Cheap as chips, but quite large.

I've come across pluggable terminal blocks but these are expensive.

 

The hardest element to find seems to be the panel mount socket (except for d-sub) but I'm not sure that I'm searching with the right keywords.  It's even harder to find a panel mount socket that is not expensive.  I'd settle for d-sub but thought I'd throw this out there for ideas.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 5 years ago

    How many pins do you need?

    How much weight or force will the connection need to support?

    How often does the connection need to be disconnected?

    Are there any other mechanical connections between panels?

    Is there motion or vibration involved?

    Do the connectors need to lock together?

    How big are the PCBs?

    PCB-mount connectors that are also bulkhead mounted exist but are over-constrained mechanically - if the pcb is screwed to the chassis and the connector is fastened to the panel, it can put stress on the solder joints. (So tight tolerances will need to be maintained)

    If the panel-to-panel connector is the only connection between modules, the connector may need to withstand high forces. Many connectors only have one side panel mounted to avoid this because they are not strong enough to support more than the weight of a cable.

    There are many through-hole board-to-board connectors that need cutouts in the panels to go between modules, but they don't usually have panel fasteners.

    The DB connectors you mentioned can do it all, but have limited strength, and it is tough to get them screwed together in the confined gap between panels.

    Many circular bulkhead connectors can be mounted to PCBs although most are vertically oriented on the PCB. Also usually pretty expensive.

    The bottom line is that what you want is not commonly available because the connectors would need to be so strong, they would be very expensive. There are many possible solutions to accommodate specific applications where some of the normal requirements are not needed, but more information is needed to tailor a solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to dougw

    Interesting and useful points Doug.  I seem to have narrowed it down to 15 pins across 3 connectors, for convenience - 2 on the back, 1 on the front.  But I could go 10, 5, 5, 5, 15. There's no vibration, shearing force or weight beyond perhaps a cable with connectors on each end as they will be linking bench top cases together.  So I might connect the rear two to two connectors on another case, ditto the front one to another case.  I don't want them permanently connected to each other, nor to open the case to connect/disconnect them.  It's all hobbyist stuff in any case so there are no standards to conform to.

     

    But also, the question was as much about working out what is out there because it seemed to be a bit of a desert and I may have been using the wrong search terms - your pointers make me think that what I'm finding is what I'm finding!! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 5 years ago in reply to Andrew J

    Andrew J if you need 15 pins why not use a DB-15 and they can be connected directly connected together one female the other male.

    ~~ Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to phoenixcomm

    I Did mention that Chris although I referenced them as D-Sub.  I quite like the idea as I can make a hard connection, or stick a cable in between if necessary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 5 years ago in reply to phoenixcomm

    I Did mention that Chris although I referenced them as D-Sub.  I quite like the idea as I can make a hard connection, or stick a cable in between if necessary.