• Products and Partners
    Products and Partners
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
Member's Forum Case to Case Connections
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 630 subscribers
  • Views 3186 views
  • Users 0 members are here
Related

Case to Case Connections

Andrew J
Andrew J over 5 years ago

I'm looking for ideas for connecting encased devices.  So PCB -> Panel <-air gap-> Panel -> PCB.  Better:  Free end (for crimping connector) -> Panel <-air gap-> Panel -> Free end (for crimping connector).  I'm just looking to transfer signals and low-current, low-voltage power in a cheap way.  Although PCB edge-mounted connectors are an available option, I can't use these.

 

An example solution would be an IDC connector with flat cable: flexible with a variety of potential contacts and easily obtained with pre-made cables.  It's easy to find PCB mounts and male/female connectors but a panel mount socket (or plug) seems non-existent.   

 

An alternative would be d-sub connectors.  Again, variety of potential contacts, easy to solder up, but quite large.  Easy to find male/female connectors as well as panel mount.  Cheap as chips, but quite large.

I've come across pluggable terminal blocks but these are expensive.

 

The hardest element to find seems to be the panel mount socket (except for d-sub) but I'm not sure that I'm searching with the right keywords.  It's even harder to find a panel mount socket that is not expensive.  I'd settle for d-sub but thought I'd throw this out there for ideas.

  • Sign in to reply
  • Cancel
Parents
  • Andrew J
    0 Andrew J over 5 years ago

    Thanks Guys.  John: there are some interesting test tools on that site but I couldn't find anything specific to panel connectors unfortunately.

     

    RJ45 is a good idea for up to 8 contacts.  The MDR connectors are very similar to the D-Sub connectors, a little smaller and using wiper contacts for IDC cables rather than pins and soldered wires; bit more expensive.  As for IDC panel connectors there are very few.  Also, micro-bayonet connectors e.g. https://uk.farnell.com/amphenol-sine-tuchel/c016-10g014-0001/socket-panel-14-pe-way/dp/1123480 although they need crimps as well.

     

    It would seem that PCB edge mount would give the most flexibility but would need to be designed with the case in mind, assuming a custom one wasn't being made (which it isn't!!)  I'm amazed that there aren't more options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to Andrew J

    Hi Andrew,

     

    I know what you mean, and sometimes it may be easier to just place all connectors on one side of the board, so it fits any enclosure, but often it's not ideal/feasible to put them all on one side.

    Another option could be to have a snap-off portion of PCB, where (say) it could have vertical DIL header and screw holes on the PCB so that the snap-off portion is screwed onto the enclosure. and then have flat flex (for example) to connect to the main board. For really low cost non-critical applications, the flat flex could just be soldered without connectors.

    This is also ideal for all sorts of connectors that are PCB-mount, and saves on wire assembly time etc.

     

    In this example (at right angles in this case however) I needed three connectors, but the main PCB wasn't designed for that, so I created a small separate custom PCB with the three connectors on it, and inside the enclosure there are JST cables going from here to the boards that require each of the connections.

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 5 years ago in reply to shabaz

    Very cool!  I really like the piggyback USB port landed opposite of the RJ45.  This is something that I will have to try sometime.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • genebren
    0 genebren over 5 years ago in reply to shabaz

    Very cool!  I really like the piggyback USB port landed opposite of the RJ45.  This is something that I will have to try sometime.