• Products and Partners
    Products and Partners
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
Member's Forum Case to Case Connections
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 630 subscribers
  • Views 3186 views
  • Users 0 members are here
Related

Case to Case Connections

Andrew J
Andrew J over 5 years ago

I'm looking for ideas for connecting encased devices.  So PCB -> Panel <-air gap-> Panel -> PCB.  Better:  Free end (for crimping connector) -> Panel <-air gap-> Panel -> Free end (for crimping connector).  I'm just looking to transfer signals and low-current, low-voltage power in a cheap way.  Although PCB edge-mounted connectors are an available option, I can't use these.

 

An example solution would be an IDC connector with flat cable: flexible with a variety of potential contacts and easily obtained with pre-made cables.  It's easy to find PCB mounts and male/female connectors but a panel mount socket (or plug) seems non-existent.   

 

An alternative would be d-sub connectors.  Again, variety of potential contacts, easy to solder up, but quite large.  Easy to find male/female connectors as well as panel mount.  Cheap as chips, but quite large.

I've come across pluggable terminal blocks but these are expensive.

 

The hardest element to find seems to be the panel mount socket (except for d-sub) but I'm not sure that I'm searching with the right keywords.  It's even harder to find a panel mount socket that is not expensive.  I'd settle for d-sub but thought I'd throw this out there for ideas.

  • Sign in to reply
  • Cancel
Parents
  • genebren
    0 genebren over 5 years ago

    Andrew,

     

    I like to use connectors that have nice pre-made cables available for them, like USB and HDMI.  While these cables may have limited connections, they are plentiful and relatively inexpensive.  One of the approaches that I have used when going from device to device to shift over to a serial bus (UART, I2C, SPI) and multiplex the data onto a minimum set of pins.  This definitely works for digital signals, but may be more problematic when it comes to power and analog signals.

     

    Another useful approach that I have used with analog/power are IDC connectors from AMP (https://www.newark.com/w/c/connectors/idc-connectors?product-range=mta-100-series ).  These come in different pitches and connector counts.  They are easy to use, with push on wires and can be used with ribbon cables for very neat cables.  Best of all they can be used with standard headers, or special locking headers.

    image

     

    Good luck!

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to genebren

    I think it's a neat idea to use connectors for a purpose other than their intended one.  I've looked long and hard at IDC but the issue is panel mount: the only way I can see of using them is to pass the cable through.  This basically means a permanent connection unless the case is opened, or creating a separate PCB to hold the connector at the edge so it can be positioned up against the case.  The difficulty with the latter is managing insertion and removal forces when only the PCB solder and, perhaps, bracing pins are available to take the strain.  You'd need something that had a low friction level I think (like USB, HDMI, DC Jacks etc..)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to Andrew J

    Hi Andrew,

     

    I'm wondering if I misunderstood your requirement.

    Wouldn't this (photo below) IDC option meet your needs? It fits to the panel, and plugs onto the PCB (or can cut the ribbon cable and solder it to the PCB).

    And then, the other device would have the exact same thing, and then they interconnect with a ribbon cable.

    By 'air gap' do you mean you wish to directly plug the two enclosures together, with no cable?

    image

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 5 years ago in reply to shabaz

    shabaz I like RJ-45s as well but if you are talking about two boxes next to each other DB-15 are perfict.

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to Andrew J

    I see.. Personally I think RJ45 is cleaner than D-Sub (for 8 or fewer connections) since the cables are ready-made and popular (can even get 25cm cables for short interconnects) whereas with D-Sub at least to me it's confusing if they are null modem or otherwise.

    Yes, these were photos found via google, on aliexpress.. it's getting crazy finding parts in stock these days.. and it was nice to see a photo with cable on the end. If it's a non-critical application then they should be good enough from Aliexpress I guess.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to shabaz

    I've been thinking of different scenarios but I don't think you misunderstood: I wasn't very specific originally as I was really just interested in seeing if there were other types of panel connectors I was unable to find.  By air-gap I just meant "physical separation of case panels".

     

    With the information that everyone has posted above I've been thinking through different approaches.  Could I have, for example, a D-Sub socket on one case and a D-Sub plug on another so I could either physically connect them together or use a cable - I may want to connect the case outputs to a plug on a PCB/breadboard setup which would require a cable.  That approach gives me some flexibility: D-Sub are cheap but large.  My first approach was to have an actual air gap with cable as it gives a degree of flexibility in positioning cases and IDC would be great for that because the cables are inherently flexible, but I struggled to actually find a panel connector!  I've been looking on Farnell as part of filling my $100 basket.  What you have shown in the photo would cover that approach - actually, aren't those connectors in the bottom image similar to the link you gave in your first answer (that one was expensive and available to manufacturer order in 47 days!!)?  I'm guessing those in your pics are Alibaba or similar?

     

    Another approach may have been to create a separate PCB (or use veroboard) and have some right-angled Molex headers with a case cutout as I already have some plugs.  Not very aesthetic though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 5 years ago in reply to shabaz

    I've been thinking of different scenarios but I don't think you misunderstood: I wasn't very specific originally as I was really just interested in seeing if there were other types of panel connectors I was unable to find.  By air-gap I just meant "physical separation of case panels".

     

    With the information that everyone has posted above I've been thinking through different approaches.  Could I have, for example, a D-Sub socket on one case and a D-Sub plug on another so I could either physically connect them together or use a cable - I may want to connect the case outputs to a plug on a PCB/breadboard setup which would require a cable.  That approach gives me some flexibility: D-Sub are cheap but large.  My first approach was to have an actual air gap with cable as it gives a degree of flexibility in positioning cases and IDC would be great for that because the cables are inherently flexible, but I struggled to actually find a panel connector!  I've been looking on Farnell as part of filling my $100 basket.  What you have shown in the photo would cover that approach - actually, aren't those connectors in the bottom image similar to the link you gave in your first answer (that one was expensive and available to manufacturer order in 47 days!!)?  I'm guessing those in your pics are Alibaba or similar?

     

    Another approach may have been to create a separate PCB (or use veroboard) and have some right-angled Molex headers with a case cutout as I already have some plugs.  Not very aesthetic though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 5 years ago in reply to shabaz

    shabaz I like RJ-45s as well but if you are talking about two boxes next to each other DB-15 are perfict.

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to Andrew J

    I see.. Personally I think RJ45 is cleaner than D-Sub (for 8 or fewer connections) since the cables are ready-made and popular (can even get 25cm cables for short interconnects) whereas with D-Sub at least to me it's confusing if they are null modem or otherwise.

    Yes, these were photos found via google, on aliexpress.. it's getting crazy finding parts in stock these days.. and it was nice to see a photo with cable on the end. If it's a non-critical application then they should be good enough from Aliexpress I guess.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer