Member's Forum What have you discovered that has improved your user experience at the new E14 Community site?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 51 replies
  • Subscribers 629 subscribers
  • Views 9738 views
  • Users 0 members are here
  • user
  • user experience
Related

What have you discovered that has improved your user experience at the new E14 Community site?

colporteur
colporteur over 4 years ago

I have been feeling disconnected from the E14Community since the move to the new site. The majority of the feelings came from actually not being able to communicate after the move. I could receive but not transmit. Making or responding to posts wasn’t possible. Rather frustrating to read stuff and no be able to respond. After being shown a work around that enabled my transmit, the communication part has been solved.

The disconnect feeling remains because things have moved and I can't find what was once familiar to me. I will continue to struggle until I can reconnect with the sources of information I had on the old site. Here are some touch points I have been using to help recover from my disconnect. 

In the past I ignored the the landing page and clicked on CONTENT All. From that site pulse point, I got a reasonable picture of changes in the environment. The CONTENT All doesn’t exist on the new site.

image

My lesson 101 to reconnect is to invest in the Landing page. I turn over the tabs of Recent Content section in the lower part of the Landing Page. The posts under these tabs are suppose to reflect some of the site content as it is updated. There are some issues with this being updated but tech support is aware and working on it. Since RoadTest are important to me, I also explore what is under the RoadTests button from the landing page.

image

My third location for content culling is the Member Area. From the landing page it is easy to navigate to the location.

image

I pursue the Recent Discussions section for details.

That is three touch points I am investing in to re-establish my connection. If you have discovered something on the new site that has helped reconnect, I encourage you to share. The faster we can discover what works, the faster our community returns.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 4 years ago

    I think if the main page would have slightly rearranged columns, and unification between the first page and the 'View more results' page so that it's all the same, then things would feel more comfortable.

    I was thinking something like this (see mockup image below), it's not much different from what there is now, just a slight re-jig, but the main thing would be to have all activity, including comments etc, all on that first page, instead of having to click on "View more results", and also strip the fonts and images, or have the image as a tiny thumbnail to the left of the Title column, so that there's no distraction running the eye down the list of titles as there is now.

    I don't know if any of this is possible, or what others think, this is just a purely selfish idea of what I'd like. Is it bad/good?

    image

    In terms of what works well, for me I really like the editor capabilities, the content looks cleaner, and the images come out sharper, and it all works pretty well for content creation I think. Although, it would be nice that a couple of the important editor tools were not buried in menus, i.e. Heading 1 should be a single click, instead of traversing Format->Formats->Headings. Also, the 'Normal' font size should be the equivalent of 'Large' font size by default for blogs and discussions I feel.. maybe it is my monitor/laptop screen issue.

    Also, the default image size width of 640 should be (I feel) 1280 instead, it's a better compromise and people will soon get used to either having the most important part of their images on the left side (since a width of 1280 means only the left side of the image is visible in blogs until users click on the image), or content creators can resize back down to 640 width if they want their entire image to appear. It could be further refined later to allow the left, centre or right portion of the image to appear at the choice of the creator, until the image is clicked by the viewer.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to shabaz

    BREAK...BREAK....

    You commented on the editor. I see your posts are large(er) print than mine. In order to do that, I have to actually go into the editor option and switch to larger. I was wondering if you figured out how to change the defaults and say make larger the default vs normal.

    I see other posts suffer from the micro print I'm using. I foget to go up the size. THe default font size needs some growth hormones in my opinion. [I made the print larger for this posts but it took effort:(]

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to colporteur

    Hi Sean,

    I had to do it manually too : ( The default is definitely too tiny, compared to other websites.The larger text is perhaps slightly too large, but it's better than tiny.

    image

    Also, this would be nice to see changed; almost every single image needs resizing, for instance it chose a default of 429 pixels across, which is only an inch or two on any modern display or phone. So, I have to bring out the calculator each time, multiply the values by two, and then sit and wait while it does something with the numbers, and then click OK. 

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago in reply to colporteur

    Hi Sean,

    I had to do it manually too : ( The default is definitely too tiny, compared to other websites.The larger text is perhaps slightly too large, but it's better than tiny.

    image

    Also, this would be nice to see changed; almost every single image needs resizing, for instance it chose a default of 429 pixels across, which is only an inch or two on any modern display or phone. So, I have to bring out the calculator each time, multiply the values by two, and then sit and wait while it does something with the numbers, and then click OK. 

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz

    I first build a page in HTML / CSS and then stick it into the editor. 

    next put in the pictures. after clicking on the picture under edit there is an option of inline -right - left

    which is the same as <p><img style="float:right;" .....> the fox

    when I style an image I also like to manage my margins: TOP RIGHT LEFT BOTTOM  margin: 0px 20px 0px 0px; is what I use for images on the right hand side. 

    ~~Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Gough Lui

    Hi Gough,

    Good point, I guess it causes that issue : ( I've raised a line spacing issue within blogs/discussions on the Feedback & Support group, but I didn't realize e-mails also then had a knock-on effect as a result of selecting the larger font : (

    Probably the Telligent guys are going to be thinking we are one fussy set of users, being so picky about our font sizes and spacing : )

    Still, it can't be helped, we just like it the way we like it : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to shabaz

    The font size tinkering may seem okay on the website - but there seems to be an issue with the line spacing (perhaps it's fixed) on the e-mail notifications, so everyone with the larger text looks like this in the e-mails:

    image

    Perhaps something cstanton might want to look into?

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to phoenixcomm

    Hi Cris,

    I hope you are having great hols time too.
    I didn't think of grabbing the corner to resize! This solves the image issue! : )

    Also, good point that we could quickly edit the HTML, I'll try that on my next discussion or blog post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz

    I also agree that the font is too small. I do most of my work in HTML so inside a paragraph use a style command in which you change everything ie. font-size font-family, etc. 

    <p style="font-size:24pt; font-color: blue; ">the dog jumped over the fox</p>

    also for resizing photos just click on it the boxes will be in its corners grab one and more diagonally. during layout, you can change where the photo is  by right, left, etc. but really I use <img style="float: right/left; margin: (look this up CSS margin see https://www.w3schools.com/

    by combining various CSS style commands you can achieve a blog.

    ~~Cris

    BTW Hope everyone had a happy, happy holiday.