Member's Forum Should Handheld multimeters have color LCD displays?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 75 replies
  • Subscribers 593 subscribers
  • Views 11130 views
  • Users 0 members are here
Related

Should Handheld multimeters have color LCD displays?

scottiebabe
scottiebabe over 3 years ago

As I am waiting for my OWON HDS242 to come in the mail, I thought I might ask other members how they feel about a handheld multimeter having a power hungry color LCD display.

The product webpage suggests a battery life of 3-6 hours. https://www.owon.com.hk/products_owon_hds200_series_digital_oscilloscope 

Even more interesting/exciting is the batteries can be recharged with a USB-C cable.

Based on Kerry Wong's teardown: http://www.kerrywong.com/2021/09/18/teardown-of-an-owon-hds272s-3-in-1-handheld-oscilloscope-dmm-awg-compared-with-hantek-2d72/ the multimeter functionality is galvanically isolated from the usb connector.

What do you think?

First time trying the poll feature, hopefully I didn't goof it!

Based on Kerry's notes the meter also has the bones of a real oscilloscope (ADC, FPGA, Sample memory, etc..) How performant is oscilloscope it? I don't know yet.... But I am intrigued!

Update: The scopemeter arrived!

Indoors the color LCD looks awesome! For me my multimeter ends up either sitting flat on my desk on in my lap and in both those cases the display is 10x easier to read than a segment LCD without a backlight.

Outdoors with direct sunlight the segment LCD is easier to read than the color LCD.

In the shade outdoors, I think both display technologies are equally legible.

image

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +6
    So.... I'd say, "yes," but, I'd rather have a higher-quality monochrome than a lower-quality color. That said if I can slightly flex, a company called Kaitweets sent me one of their meters. These are…
  • Jan Cumps
    Jan Cumps over 3 years ago +4
    I voted Yes! although I don't know why I'd need it yet. In other instruments, colour has often been a gimmick in the beginning. But then real good use was found for it. I put my money on this: "in a…
  • dang74
    dang74 over 3 years ago +4
    I voted yes, but it was in context to the additional information that was provided, namely that in this case it's perfectly acceptable because the product also doubles as an oscilloscope. Should all manufacturers…
  • colporteur
    colporteur over 3 years ago

    How would individuals with colour blindness be impacted on colour display meters?

    I think I see all the spectrum of colour. I worked with an individual that didn't identify the colour red. To him it was black. Red & black being two colours in a single pair cable gave him a 50/50 chance of getting the pair connected correctly. After understanding his colour shortcoming we came to an agreement. I would terminate cables and he drove the truck. As electronic installers terminating 250 pair cables was a regular occurrence. Not seeing red made terminating cables difficult.

    Do meters that support colour offer an override option to set the output to monochrome? If John and I still worked together I can hear him now "Who set this GD meter to colour! No wonder I can read the numbers."

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to colporteur

    I am fortunate that is not an issue that applies to me, but you are absolutely correct this is an important topic for consideration. Perhaps the meter should allow the user to chose a color scheme.

    There are a few thermalcamera-multimeters that also have color displays. The Fluke 279 and FLIR DM166, they both seem to use a white on black or black on white display font when in multimeter mode. (I haven't used either)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    Re: Battery Life. I would not want to have to take my multimeter apart all the time to charge the battery like the Fluke 279 thermalcam multimeter:

    image

    That would bother me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

     scottiebabe , is this the same one: MP720780 ?

    I have a shopping cart from project14. May pick this one ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    I can't say for certain but if I had to guess I would say yes! That is exciting news!! You may also consider the model with an AWG included 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    I ordered one of that family. MP720783

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    Nice specs! Looking forward to hearing what it's like.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Woohoo! Sparkle I am excited for you! We are twins for Scopes (DS1054z), I have the big sister to your function generator and now you have the big brother to my scopemeter! Excellent choice, can't wait to hear your opinion of the meter:)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to scottiebabe

    Funny you mention this ... I've just reviewed the Fluke 279 FC/iFlex -  Experimenting with Thermistors – Grand Prize Pt.2: Fluke 279 FC/iFlex DMM Review

    Using that as my reference point for a colour LCD DMM, I guess the 279 FC/iFlex has no choice as the thermal imager really needs a colour LCD to truly shine. But the colour LCD is a compromise - for use outside in direct sun, its contrast is barely enough for reading DMM digits. Power consumption means that the lifetime of a 22Wh battery is only about 13-14h so charging becomes necessary (although if not using continuously, you can still get quite a bit of mileage). Unfortunately, the 279 FC/iFlex doesn't make the most of the LCD either - colour is only used for the "danger" icon, and there is no bar graph as you may see with segment mono LCDs.

    In the end, for a plain DMM, I still find monochrome segment LCDs preferable - they're just more readable in more situations (backlights help in the dark) and they consume much less power. Simple technology, low-cost ... nothing wrong with that.

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    My scope arrived!

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<>