• Products and Partners
    Products and Partners
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
Member's Forum New Here & 1st Problem!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 629 subscribers
  • Views 4128 views
  • Users 0 members are here
  • opamp
  • comparator
  • lm393
Related

New Here & 1st Problem!

Gosling616
Gosling616 over 3 years ago

I am going back to my youth as an electronic engineer to design some stuff. 

I have joined hoping for help. 

This will be the start of a few minor project around building a cockpit for online flying. Basically, Arduino boards loaded with code and game libraries to detect game events. Coding is a new area for me. I’m pre PCs back then

Anyway, my current problem is more descrete. 

With Vcc at 5V and Gnd at 0v, why does my LM393N Op Amp output 0.7v when I/P 1(-) is connected to Gnd and I/P 1(+) is 2.5V by connecting to the middle of 2 x 5kOhm in series across Vcc and Gnd???

I was hoping to get 5V O/P to drive a MOSFET Board for a 12v power control over a magnetic field coil…

  • Sign in to reply
  • Cancel
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Welcome. You will get answers here. There is a lot of knowledgeable people around. 

    The LM393 output is an open collector type. You would need a pull-up resistor to Vcc to get a proper high level. Like so (from the TI LM393 datasheet):

     image

    And the LM393 is a comparator, not a full op-amp. Just in case you plan to do more analog stuff with it.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to wolfgangfriedrich

    Thanks.  Just what I needed - I’ll give that a go and see what happens.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gosling616
    Gosling616 over 3 years ago in reply to wolfgangfriedrich

    Thanks.  Just what I needed - I’ll give that a go and see what happens.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago in reply to Gosling616

    Cheers. From the results, it sounds like there is a pull-down resistor on that signal on the MOSFET board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to Gosling616

    I tried a 2k and it draws the signal to Hi, but once I connect it to the MOSFET board the signal goes low.  I worked the R Value down to 660Ohm using three x 2k and that works now.  Thanks..