• Products and Partners
    Products and Partners
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
Member's Forum New Here & 1st Problem!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 629 subscribers
  • Views 4128 views
  • Users 0 members are here
  • opamp
  • comparator
  • lm393
Related

New Here & 1st Problem!

Gosling616
Gosling616 over 3 years ago

I am going back to my youth as an electronic engineer to design some stuff. 

I have joined hoping for help. 

This will be the start of a few minor project around building a cockpit for online flying. Basically, Arduino boards loaded with code and game libraries to detect game events. Coding is a new area for me. I’m pre PCs back then

Anyway, my current problem is more descrete. 

With Vcc at 5V and Gnd at 0v, why does my LM393N Op Amp output 0.7v when I/P 1(-) is connected to Gnd and I/P 1(+) is 2.5V by connecting to the middle of 2 x 5kOhm in series across Vcc and Gnd???

I was hoping to get 5V O/P to drive a MOSFET Board for a 12v power control over a magnetic field coil…

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    colporteur over 3 years ago

    Don't you just hate when someone responds with an alternative and not a reply your question.

    image

    I have had great success using this little module to drive 12VDC loads. Do a search for MOSFET driver module on part sites and you should get a hit.

    Oh yeah, welcome!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to colporteur

    Thanks, I am using this MOSFET board - £0.09 37% Off | 5PCS Top Mosfet Button IRF520 Mosfet Driver Module For Arduino MCU ARM Raspberry Pi 3.3v-5V IRF520 Power MOS PWM Dimming LED
    https://a.aliexpress.com/_mqCTYeW

    Problem I have is it needs a Vcc to switch on and so I need to convert the Gnd signal the switch gives to a Vcc, hence using the Comparator to Invert the signal.  

    But thanks anyway…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to Gosling616

    The mosfet module you are using is similar to the one I have selected other than mine has two mosfets for driving.

    image

    I blocked diagram what I think you are trying to accomplish. Can you confirm if this is correct?

    image

    You have in an external input that is low when triggered. You want to use that low to trigger a mosfet driver that requires a high to trigger. Your plan is to accomplish the signal inversion using a comparator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to colporteur

    That is correct..  I have applied a 660Ohm pull up resistor as suggested above and it now works.  Clearly the MOSFET board was pulling the O/P voltage down.  660 seems a good compromise

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gosling616
    Gosling616 over 3 years ago in reply to colporteur

    That is correct..  I have applied a 660Ohm pull up resistor as suggested above and it now works.  Clearly the MOSFET board was pulling the O/P voltage down.  660 seems a good compromise