I am an inventor I had a perfect idea so I designed and made it work the kinks out of it and has been operating now two years. It's time to get out here is my problem I have no clue how or even the finance to do anything
I am an inventor I had a perfect idea so I designed and made it work the kinks out of it and has been operating now two years. It's time to get out here is my problem I have no clue how or even the finance to do anything
Another place to look is government programs. In Canada there is an Industrial Research Assistance Program and there are usually small business development agencies and export development agencies, etc.
There are any number of web site development services that will setup an online business.
This design, that involves groundwork, cabling, installation and adaption to local (and regularly evolving) garbage can counts and sizes, may be better suited for local business.
It's a great idea and well executed. I don't think there's unique invention that can be patented and then monetised.
In Australia the lift on a bin truck will max out at 75kg will lift 85kg so I did upgrade the whole system to lift 1500kg. The hydraulic systems runs a 5000kg ram yes it over kill but I did have the same concern most people do the right thing but there all ways one.
my thoughts on what to do in the UK may be of limited use.
As a person also in the UK I looked at it and thought "That's going to struggle when the brown bin is full of soil and the recycle bin is full of glass, and the black bin is also full of glass because people have filled the other bin".
How is this protected from the rains? I live in an area where all the recycling bins are underground but waterproof. To empty them, a crane truck extracts the container from the ground and opens it on the truck with a mechanism. I don't see how your design solves the rain problem.
I like that Idea better sell it off to a bigger company
It's not a bad idea !
If you are in Auustralia my thoughts on what to do in the UK may be of limited use.
If you are going to talk to money people you need to be sure your idea is protected before you start.
In the UK I'd contact double glazing companies - because they have the infrastructure to market and install such a product. Installation is key here - I doubt if it's really a DIY product.
Where I live (very rural SW Scotland) our problem is that we have to leave bins at the end of little tracks with1 - 10 houses and the bin lorry can't/won't drive up the track. The great gaggle of bins looks bad and attracts animals. But I can't see your system going in there due to power and other considerations.
But in up-market conservation area type towny places - I think you could make some sales. The BIG effort is building the business.
If I were you I'd be really happy to sell the patent to a big company for for the price of a decent (new) car and move on to the next idea.
MK