Products
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
Member's Forum Do you have a right to privacy of your source code?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 54 replies
  • Subscribers 625 subscribers
  • Views 6773 views
  • Users 0 members are here
  • privacy
  • programming
  • copyright
  • code
Related

Do you have a right to privacy of your source code?

cstanton
cstanton over 3 years ago

As an individual, if you write a program and share the binary of that, should the expectancy be that you share its source code?

You might not want to share the source code, for example, you can very easily be judged based on that source code, both professionally and personally.

I've known people purposefully not post their code on Git Hub because they know employers will scrutinize and judge it, and in fact others observe how many 'regular commits' you do. Whether or not such judgment is fair is out of scope, but it's certainly something that's in the public eye at that point.

So perhaps you release a compiled binary because you want to help, but you don't want to invite conversations about the code, make it publicly displayed, or maybe there are other reasons.

However, someone comes along, decompiles the binary, reverse engineers it with ida pro, and releases the source code - citing that they have every right to do that, and now everyone can see the code, even though it's against your wishes.

Who was in the wrong? Or was no one in the wrong? Does it go to copyright since there was no license? Or was there an implied license?

There certainly appears to be a strong sense of justice among those online, that insists "it's just code" and "there's a right to transparency".

But there feels like there's something here that may not stand up to this scrutiny and this cavalier attitude of someone's work. Comparatively in the art world, someone creates a piece of art, and recently those components are being re-used in the case of AI (stable diffusion) and there's an uproar, but aren't they just laying the components bare? Maybe the analogy doesn't quite fit, but it certainly feels like for some reason code, by some, is treat differently to other mediums. Even though there are patents, copyrights, licenses, etc.

It could be difficult or even impossible for an individual to do something about this without financial backing, too. Especially compared to companies.

What do you think?

Edit: If you're picking up on spelling errors rather than the topic and context of the post, you're easily distracted. ;)

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 3 years ago

    My understanding....

    Source code is automatically copyrighted and you have control over how the work is used. If you don't register it with a copyright office, it gets harder to prove ownership, but doesn't change your rights to the work.

    I'm not a fan of it, but that is how it is.

    If some source code is reconstructed from some binary and altered enough, it would be hard to prove it was copied, but if proven to be a copy, it would not be legal.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller over 3 years ago in reply to dougw

    I'm not sure that's the case: copyright covers the expression but not the actual idea (for that you need a patent). So if you've copyrighted some source code and it's transformed in a way that is not just language translation then I don't think it would be covered by copyright. Thus source -> binary -> source would probably generate a new "work" for copyright purposes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bradfordmiller
    bradfordmiller over 3 years ago in reply to dougw

    I'm not sure that's the case: copyright covers the expression but not the actual idea (for that you need a patent). So if you've copyrighted some source code and it's transformed in a way that is not just language translation then I don't think it would be covered by copyright. Thus source -> binary -> source would probably generate a new "work" for copyright purposes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to cstanton

    If the symbol table was removed at compile time then I would expect you to lose your variable and function names, so you would end up with substitute names in the decompiled source.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to beacon_dave
    beacon_dave said:
    Presumably it was compiled with debug information included ?

    Not explicitly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to cstanton

    Presumably it was compiled with debug information included ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to beacon_dave
    beacon_dave said:
    If you decompile from a binary then you are likely to get a source that includes all the optimisations that the compiler included when compiling. So it will look very different (

    I had a recent exact example of this.

    A compiled binary I had shared was reversed, and it produced the exact same source code as was used to create it.

    Character for character. It wasn't an overly complex piece of code.

    It appears this varies depending on the compiler and tools used, and the intention to obfuscate Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to cstanton
    cstanton said:
    Is it a new work if it looks exactly the same and does the same function?

    You and I could both write a 'blinky' sketch that performs the same functionality. We'd each automatically have copyright on our version of the source code. 

    Now decompile each binary and compare the source.

    cstanton said:
    It's possible to get that from decompiling back to the source.

    If you decompile from a binary then you are likely to get a source that includes all the optimisations that the compiler included when compiling. So it will look very different (and often appear to do things in strange ways just because it takes less clock cycles to do it that way).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to bradfordmiller
    bradfordmiller said:
    Thus source -> binary -> source would probably generate a new "work" for copyright purposes.

    Is it a new work if it looks exactly the same and does the same function? It's possible to get that from decompiling back to the source.