Products
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
Member's Forum python code for raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 627 subscribers
  • Views 1321 views
  • Users 0 members are here
  • python programming
  • audio
  • python 3.7
  • raspberrypi
  • python code
  • software
Related

python code for raspberry pi

fskrzycki
fskrzycki over 3 years ago

# Music starts after sudo reboot, but not at initial power up.
# When audio file plays. It plays at 2x speed.
# I tried using pydub to correct the speed, but I think it conflicts with my audio card because nothing plays when I add the code. This mp3 file does play at normal speed when selected with a regular audio player

please suggest a solution

Start-up-music-for-Raspberry-Pi
#music plays when headless starts up.
# This is the location of my service file ( /etc/systemd/system/opening_audio.service)
# opening_audio.service
[Unit]
Description=plays Let It Rip when powered on

[Service]

ExecStart=/usr/bin/python /home/Bay/Bookshelf/play_mp3.py
Restart=always
User=Bay

[Install]
WantedBy=multi-user.target

#This is the Program ( Play_mp3.py )

import pygame
import time

pygame.mixer.init()
pygame.mixer.music.load("/home/Bay/Music/letitrip.mp3")
pygame.mixer.music.set_volume(0.5)
time.sleep(3)
pygame.mixer.music.play()
pygame.time.delay(9000)
pygame.mixer.music.stop()
pygame.quit()

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 3 years ago in reply to fskrzycki

    "I dont understand running it manually. I want it to start as automatically with the Pi receives power. "

    I presume that's a reply to me?

    I understand that you wished to run it automatically, this was obvious. It's part of the process of troubleshooting to narrow down the problem. The suggestions listed above are things intended to get closer to understanding the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to Gough Lui

    I should be able to change encoding parameters with Audacity. I did use it to convert the file from a wav to mp3.  I dont understand running it manually. I want it to start as automatically with the Pi receives power. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    Perhaps you might want to check the encoding parameters of your MP3 file in case it is the cause.

    I'd recommend any constant bit rate at 48kHz Stereo as that tends to avoid issues.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    In case you don't get a better answer: it could be any number of things, there's some self-troubleshooting that will be needed. Without the troubleshooting, the "hack" way would be to record an MP3 file with slowed-down audio (using, say, Audacity), but it's not what I would recommend. Instead, you just need to work through the problem.

    It could be a bug in pygame, or could be a problem with the driver (I recall you had issues locating it, and maybe there's a chance there's some slight incompatibility with it). You are using an OTT sound card board, and with it comes more complexity in the drivers.

    You could try running your code manually (i.e. not using systemd) to see if it makes a difference.

    You should also try an MP3 file with different encoding parameters to see it that helps.

    You could also try playing a .wav file in case that makes a difference too.