Products
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
Member's Forum python code for raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 627 subscribers
  • Views 1323 views
  • Users 0 members are here
  • python programming
  • audio
  • python 3.7
  • raspberrypi
  • python code
  • software
Related

python code for raspberry pi

fskrzycki
fskrzycki over 3 years ago

# Music starts after sudo reboot, but not at initial power up.
# When audio file plays. It plays at 2x speed.
# I tried using pydub to correct the speed, but I think it conflicts with my audio card because nothing plays when I add the code. This mp3 file does play at normal speed when selected with a regular audio player

please suggest a solution

Start-up-music-for-Raspberry-Pi
#music plays when headless starts up.
# This is the location of my service file ( /etc/systemd/system/opening_audio.service)
# opening_audio.service
[Unit]
Description=plays Let It Rip when powered on

[Service]

ExecStart=/usr/bin/python /home/Bay/Bookshelf/play_mp3.py
Restart=always
User=Bay

[Install]
WantedBy=multi-user.target

#This is the Program ( Play_mp3.py )

import pygame
import time

pygame.mixer.init()
pygame.mixer.music.load("/home/Bay/Music/letitrip.mp3")
pygame.mixer.music.set_volume(0.5)
time.sleep(3)
pygame.mixer.music.play()
pygame.time.delay(9000)
pygame.mixer.music.stop()
pygame.quit()

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    In case you don't get a better answer: it could be any number of things, there's some self-troubleshooting that will be needed. Without the troubleshooting, the "hack" way would be to record an MP3 file with slowed-down audio (using, say, Audacity), but it's not what I would recommend. Instead, you just need to work through the problem.

    It could be a bug in pygame, or could be a problem with the driver (I recall you had issues locating it, and maybe there's a chance there's some slight incompatibility with it). You are using an OTT sound card board, and with it comes more complexity in the drivers.

    You could try running your code manually (i.e. not using systemd) to see if it makes a difference.

    You should also try an MP3 file with different encoding parameters to see it that helps.

    You could also try playing a .wav file in case that makes a difference too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    In case you don't get a better answer: it could be any number of things, there's some self-troubleshooting that will be needed. Without the troubleshooting, the "hack" way would be to record an MP3 file with slowed-down audio (using, say, Audacity), but it's not what I would recommend. Instead, you just need to work through the problem.

    It could be a bug in pygame, or could be a problem with the driver (I recall you had issues locating it, and maybe there's a chance there's some slight incompatibility with it). You are using an OTT sound card board, and with it comes more complexity in the drivers.

    You could try running your code manually (i.e. not using systemd) to see if it makes a difference.

    You should also try an MP3 file with different encoding parameters to see it that helps.

    You could also try playing a .wav file in case that makes a difference too.