Products
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
Member's Forum Best device(s) for this cosplay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 627 subscribers
  • Views 3928 views
  • Users 0 members are here
  • cosplay
  • raspberry pi
  • Metroid
  • Samus
Related

Best device(s) for this cosplay

Amethyst
Amethyst over 3 years ago

I'm assuming many of us here are gamers, and I don't have a better clue where I'd put this. I plan to make a Samus cosplay, from Metroid. Not dedicated to one yet, but thinking Varia suit. 

I have honestly been planning this for many years, but funding left me lacking. On that note, I'm thinking of a Patreon or something, but not sure what rewards would be. Off-topic from the site, but feel free to give ideas!

For the main topic, I'd previously planned to use a mini RasPi and maybe a PICAxe, but an restarting my design with a clearer head:  but I fell behind on tech and don't know what's available. Here's the list I'd like to try to include if you have clever ideas to add, I'm all ears!

-An intake and exhaust fan in the helmet, like RasPi mini fans (5v), for temperature and breathing. I plan to fit these in the "ears" of the helmet that the hoses attach to.

-Some kind of screen in the helmet that can tell me information from the board. Looking at battery level, temperature, and possibly proximity sensor information.

I'm not sure how I can implement this though. I was previously thinking of an oLED display in the past, but they were expensive. I'm wondering if it's possible to create a reflection display off the helmet "glass" (acrylic) over the face? I've seen it work on car windshields, but what am I looking for?

-Some kind of "life form" detection I can use, eg infrared or other ideas? I would feed that input into my display.

Arm Blaster:

-Ice Beam using compressed air, unless there's a good electronic alternative? 

-Ping pong or Airsoft pellets. Which would be cheaper to build? Doesn't need to be high pressure, of course. 

-Fireballs by flash paper and cotton with a glow plug. Suggestions on safest way to control it? Not sure I want a 12v stepper in my arm cannon, not sure if a lower voltage would do the job?

Overall, what electronics do you think are the best ideas to try for something like this that's generally low power, but collectively can be demanding?

The suit is planned to be built with overlapping panels, eg outer thigh strapping over inner thigh armor. I will probably hot glue the wires on the outside of the lower layers and use connectors for LED wiring and any possible sensors I may use (eg motion sensor for behind me). Looking for what your experience is on best budget connectors for that.

image

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    I have no idea what this thread is about.. but I'm alright with that!

    I saw some mention of projectors.. I picked up this thing, it was so cheap. It's very likely LCD-based, not DLP at this price.

    image

    I wasn't expecting much, just something fun for kids to play with. However, it's a bit stinky (literally) in that it gets hot and smells!

    I would like to open it but it is either glued shut, or is very tightly clipped together.

    The image quality was better than expected! It doesn't work with all HDMI sources (maybe I need to set the source resolution) but this was from my Samsung phone's USB-C-to-HDMI connection, playing a video:

    image

    That was taken with the projector about 2.5 or 3 meters away from a slightly tinted wall. not quite white, and with room lights off since obviously it cannot output a lot of light. The image was slightly larger than the camera took (I had a portrait lens).

    I wouldn't leave this thing on unattended or near clothing.. there's an excellent chance it would catch fire... or burst if one chooses the Lithium-Polymer powered version. 

    In summary it is just an (unsafe) toy, but nevertheless image quality is better than what I had expected.. about as watchable as an old standard-definition TV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    I have no idea what this thread is about.. but I'm alright with that!

    I saw some mention of projectors.. I picked up this thing, it was so cheap. It's very likely LCD-based, not DLP at this price.

    image

    I wasn't expecting much, just something fun for kids to play with. However, it's a bit stinky (literally) in that it gets hot and smells!

    I would like to open it but it is either glued shut, or is very tightly clipped together.

    The image quality was better than expected! It doesn't work with all HDMI sources (maybe I need to set the source resolution) but this was from my Samsung phone's USB-C-to-HDMI connection, playing a video:

    image

    That was taken with the projector about 2.5 or 3 meters away from a slightly tinted wall. not quite white, and with room lights off since obviously it cannot output a lot of light. The image was slightly larger than the camera took (I had a portrait lens).

    I wouldn't leave this thing on unattended or near clothing.. there's an excellent chance it would catch fire... or burst if one chooses the Lithium-Polymer powered version. 

    In summary it is just an (unsafe) toy, but nevertheless image quality is better than what I had expected.. about as watchable as an old standard-definition TV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Amethyst
    Amethyst over 3 years ago in reply to shabaz

    Thanks for trying to help! Thing is, I'm looking for a small one that I can fit into a helmet, to create a HUD, potentially by a "pepper's ghost" type of effect.