Products
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
Member's Forum AM & FM differences...still learning after 27 years
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 628 subscribers
  • Views 1179 views
  • Users 0 members are here
  • modulation
  • radio frequency
Related

AM & FM differences...still learning after 27 years

colporteur
colporteur over 2 years ago

I worked in aviation for seventeen years and never heard of this Amplitude Modulation (AM) and Frequency Modulation (FM) anomaly. 

https://www.rtl-sdr.com/demonstrating-the-fm-capture-effect-why-aircraft-use-am/

I challenge the supposition it is the reason why aviation is still using AM. If that had some bearing then Marine frequency wouldn't use FM.

27 years ago my career path took a forked that moved from aviation electronics to system administration. I still treasures the memories of RF waves.

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 2 years ago

    Well, I'd say it's a complex set of reasons ...

    The first is probably for legacy reasons - it's not easy to force everyone to change-over to another system, especially one that is multinational. Aviation has been around for a long time, and the predominant technology at the time of conception was likely AM, so it's "stuck". That being said, FM has its benefits for lower-cost, higher-powered transmissions as linearity is not a major concern.

    The second is likely to do with multiple signals simultaneously on the air (getting "stepped on"). AM modulation can handle multiple transmissions overlapping and still be intelligible. FM modulation, however, does one of two things - where the frequency is within "capture" range and the signal is strong, the demodulator tracks the stronger signal while rejecting the weaker one significantly (meaning you will hear just one, but not the other). Or, if the signals are very close together and similarly strong, it breaks down into a heterodyne "squeal" which is quite unpleasant to listen to but will also block out both transmissions without much way to identify each.

    Because planes are in the air and frequencies are re-used across different airports and across jurisdictions, the possibility of having competing signals at vastly different strengths is more likely than for a ground-based system. Furthermore, VHF band transmissions can be vulnerable to very occasional summer-time sporadic-E tropospheric ducting events which increase the range of signals dramatically compared to the normal "limited-by-horizon" range.

    Another issue may be related to how the signal-to-noise ratio of the demodulated output degrades as a function of input signal to noise ratio. AM generally works down to quite weak signals and tends to degrade "gracefully" into static. FM, on the other hand, tends to be very good up to a point and then fails more rapidly into white-noise static (as far as I can tell). Perhaps this gives some reassurance about the reliability of the communication channel.

    Of course, in a perfect world, high-quality vocoder compression and a digital-radio with copious amounts of error correction will achieve further ranges with the same quality (think of digital mobile phones compared to analog mobile phones or digital radio versus analog radio, noting that in most countries, digital radio is being broadcasted at 1% to 10% of the power used by analog radio), but it's also a level of complexity that may make it more liable to failures, more difficult to service and a difficult proposition to get the world to change over to.

    Definitely a good question to think of, as most land-based systems have long eschewed AM and FM for digital-modulations (e.g. BPSK/QPSK-variants) carrying error-corrected compressed digital audio (e.g. P25, TETRA, dPMR/DMR/NXDN/iDAS/MotoTrbo). Ironically, AM and FM mainly live on in the amateur radio world (where digital alternatives like D-STAR only have limited success) and in low-cost walkie-talkie (CB) type applications. For many radio planning authorities, they operate along the ethos of  "Bandwidth is a limited resource - spectral efficiency is king".

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 2 years ago

    Well, I'd say it's a complex set of reasons ...

    The first is probably for legacy reasons - it's not easy to force everyone to change-over to another system, especially one that is multinational. Aviation has been around for a long time, and the predominant technology at the time of conception was likely AM, so it's "stuck". That being said, FM has its benefits for lower-cost, higher-powered transmissions as linearity is not a major concern.

    The second is likely to do with multiple signals simultaneously on the air (getting "stepped on"). AM modulation can handle multiple transmissions overlapping and still be intelligible. FM modulation, however, does one of two things - where the frequency is within "capture" range and the signal is strong, the demodulator tracks the stronger signal while rejecting the weaker one significantly (meaning you will hear just one, but not the other). Or, if the signals are very close together and similarly strong, it breaks down into a heterodyne "squeal" which is quite unpleasant to listen to but will also block out both transmissions without much way to identify each.

    Because planes are in the air and frequencies are re-used across different airports and across jurisdictions, the possibility of having competing signals at vastly different strengths is more likely than for a ground-based system. Furthermore, VHF band transmissions can be vulnerable to very occasional summer-time sporadic-E tropospheric ducting events which increase the range of signals dramatically compared to the normal "limited-by-horizon" range.

    Another issue may be related to how the signal-to-noise ratio of the demodulated output degrades as a function of input signal to noise ratio. AM generally works down to quite weak signals and tends to degrade "gracefully" into static. FM, on the other hand, tends to be very good up to a point and then fails more rapidly into white-noise static (as far as I can tell). Perhaps this gives some reassurance about the reliability of the communication channel.

    Of course, in a perfect world, high-quality vocoder compression and a digital-radio with copious amounts of error correction will achieve further ranges with the same quality (think of digital mobile phones compared to analog mobile phones or digital radio versus analog radio, noting that in most countries, digital radio is being broadcasted at 1% to 10% of the power used by analog radio), but it's also a level of complexity that may make it more liable to failures, more difficult to service and a difficult proposition to get the world to change over to.

    Definitely a good question to think of, as most land-based systems have long eschewed AM and FM for digital-modulations (e.g. BPSK/QPSK-variants) carrying error-corrected compressed digital audio (e.g. P25, TETRA, dPMR/DMR/NXDN/iDAS/MotoTrbo). Ironically, AM and FM mainly live on in the amateur radio world (where digital alternatives like D-STAR only have limited success) and in low-cost walkie-talkie (CB) type applications. For many radio planning authorities, they operate along the ethos of  "Bandwidth is a limited resource - spectral efficiency is king".

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • robogary
    robogary over 2 years ago in reply to Gough Lui

    Thanks - a good job explaining getting "stepped on"  :-)   I wonder if legacy is the main driver. There are lots of big aircraft , and also small aircraft and airports with existing equipment. Unless there is some huge advantage of one over the other , or governments intervention, its not likely to change. An example, the USA started a move in the late 60s and 70s to metric, useage driven by imported and exported equipment. I have 2 sets of wrenches, screwdrivers, allen wrenches, etc....one metric, one english/imperial. 

    Interestingly enough, FM radios come in analog and digital flavors too. :-)