Products
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
Member's Forum LoRa or wifi ..... max received signal strength -20bBm?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 626 subscribers
  • Views 1873 views
  • Users 0 members are here
Related

LoRa or wifi ..... max received signal strength -20bBm?

davebullockmbe
davebullockmbe over 2 years ago

Can someone explain why no matter how close I place my two Lora evaluation modules next to one another (or my phone to my wifi hub) I never achieve a signal strength higher than -20dBm?

Is there some form of AGC in the receivers that prevents the input from exceeding -20dBm input, or do the TX/RX combinations communicate with each other to throttle back the TX power?
I have been bemused by this when fiddling with wifi in the past,  but now I find that Lora is exhibiting the same behaviour despite the specified TX power being much greater and the antennas almost touching one another.. 
Clearly I am missing something? 
Can someone point me to the idiot's guide as to why this is occurring please?

Thanks
Dave

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 2 years ago

    -20 dBm is very high received signal strength.

    Antennas are not designed to be used so close-up incidentally (they need a bit of distance for the electromagnetic radiation to do it's thing (plus, it de-tunes them), and again, if you're seeing -20 dBm, that's very strong for all typical receivers).

    Also, there will be some AGC (in most typical receivers, although the cheapest may omit it).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago

    -20 dBm is very high received signal strength.

    Antennas are not designed to be used so close-up incidentally (they need a bit of distance for the electromagnetic radiation to do it's thing (plus, it de-tunes them), and again, if you're seeing -20 dBm, that's very strong for all typical receivers).

    Also, there will be some AGC (in most typical receivers, although the cheapest may omit it).

    • Cancel
    • Vote Up +3 Vote Down