Products
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
Member's Forum LoRa or wifi ..... max received signal strength -20bBm?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 626 subscribers
  • Views 1873 views
  • Users 0 members are here
Related

LoRa or wifi ..... max received signal strength -20bBm?

davebullockmbe
davebullockmbe over 2 years ago

Can someone explain why no matter how close I place my two Lora evaluation modules next to one another (or my phone to my wifi hub) I never achieve a signal strength higher than -20dBm?

Is there some form of AGC in the receivers that prevents the input from exceeding -20dBm input, or do the TX/RX combinations communicate with each other to throttle back the TX power?
I have been bemused by this when fiddling with wifi in the past,  but now I find that Lora is exhibiting the same behaviour despite the specified TX power being much greater and the antennas almost touching one another.. 
Clearly I am missing something? 
Can someone point me to the idiot's guide as to why this is occurring please?

Thanks
Dave

  • Sign in to reply
  • Cancel
  • davebullockmbe
    davebullockmbe over 2 years ago in reply to acdc90

    Phone as a test instrument?
    Not really, just as a demonstration to test my notion that these devices seem to ignore the laws of physyics once a certain signal strength has been reached.
    Where a simple signal strength meter will display stronger and stronger signal the closer one gets to the signal source, readings around -20dBm seem to be the limit when testing with LoRa modules or a mobile phone.
    It was just bothering me as to why the signal strength appeared to limit.
    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • acdc90
    acdc90 over 2 years ago in reply to HKPhysicist

    it sounds like you are using your phone as a test instrument 

    when you want results of a spectrum analyzer 

    with out the right gear your result is still " hear say " 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • HKPhysicist
    HKPhysicist over 2 years ago

    Your meter has overflown.  Your meter is a digital instrument which has an effective range of reading.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to kmikemoo

    Also some of the radio chips are so complicated, that it's easy to wrongly compute the measurement, or display a measurement that has not been adjusted to compensate for all the settings.

    I don't know what LoRa chip is being used, but the (extremely popular) SX1276 has (seemingly unresolved) comments on the Internet concerning how to translate register values into a dB value. Some people reporting discrepancies in the multiple tens of dB. For that chip at least, the formula depends on if it's LoRa or FSK (the chip can perform both options), and on the SNR value reported in a different register, and whether per-packet measurements are being used (which for some reason are inaccurate) or a non-packet measurement (yet again, a different register for that), plus it's dependent on an amplifier gain setting. Plus there's an error in linearity noticeably at large signal levels for that chip apparently. But I don't know what chip is being used, nor what software, so someone might need to also do that investigation, and perhaps change register values to see the effect, if it was really important to get to the bottom of it. And doing all that, the value is still meaningless if the two antennas are right next to each other.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to davebullockmbe

    Just guessing here, but -20dB in radio is 100uV.  Maybe there's a clamping circuit in the chip to keep the front end from being overloaded.  With it being consistent, it's got to be a feature - not a coincidence.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to davebullockmbe

    There's no reason for it to be -20 dBm, any more than 0 dBm. Zero isn't a reference value, it's just a power level that happens to be written as a zero. You noticed your WiFi signal was -25, so that's a different value too.

    It's too simplistic to try to match it to a log rule not just because of reflections, but also because the antenna detunes itself when it's held extremely close. It depends on the antenna design. Plus WiFi is a protocol, it's not just an unmodulated CW signal, and signal level might adapt (I'm no WiFi expert).

    One reason why the reporting could be a round number (instead of say -21.5 dBm) is that the chip or driver or software might not be reporting it with any better granularity. 

    Here's a screenshot from my WiFi access point, with a mobile phone held close to it. The value is -16, again no reason for it to be specifically -20 or -25 or 0. 

    If the aim is to check the antenna quality, it won't be any good to do it so close up. You'd either have to accept the manufacturer's spec (assuming it is attached correctly) or try to do partial measurements to ensure it is matched as best as you can make it (which again doesn't give you any specific signal strength, since all bets are off when you're measuring so close) or you could try to do a DIY field test of some sort (because full antenna testing costs five-figure sums, at least).

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davebullockmbe
    davebullockmbe over 2 years ago in reply to anniel747

    Hi thanks for your replies.

    Yes but WHY -20dBm ?
    What scientific principle limits receivers to only report -20dBm no matter how strong the field strength?
    I just tested my mobile phone running 'wifi analyser' app. near my wifi hub and from about 40cm to right against the hub the signal never wavered from -25dBm. A normal CW signal would have varied logarithmically as expected according to the laws of physics (ignoring multipath!)
    What anomaly of physics are these devices employing to "defy the laws of physics Jim"?
    Joking aside, I know -20dBm is recognised as a strong signal, but why -20dBm and not 0dBm or +20dBm.
    I have mostly measured RF power referenced to zero dBm so what's going on?
    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago

    ADR function.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    -20 dBm is very high received signal strength.

    Antennas are not designed to be used so close-up incidentally (they need a bit of distance for the electromagnetic radiation to do it's thing (plus, it de-tunes them), and again, if you're seeing -20 dBm, that's very strong for all typical receivers).

    Also, there will be some AGC (in most typical receivers, although the cheapest may omit it).

    • Cancel
    • Vote Up +3 Vote Down