Products
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
Member's Forum Is electronic engineering dead?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 627 subscribers
  • Views 3715 views
  • Users 0 members are here
  • ic designers
  • integrated circuit designers
  • electronic engineering
  • fpga
  • student question
  • hardware design
Related

Is electronic engineering dead?

cstanton
cstanton over 2 years ago

I saw this question on Reddit, and I figured it was a good one to ask the element14 Community as a thought provoking query that may be on new engineering students minds:

"If we consider only circuit design for PCBs, almost all the complexity is moving toward integrated circuits (chip and modules) and/or in code for FPGA or microcontrollers/microprocessors. The role of hardware engineers is still important, because of PCB layout and BOMs, but from the hardware design point of view is almost all already done, just pick a component, read the datasheet and copy the reference design. I’m simplifying, I know, finding the right component is not easy at all, but it seems the hardware engineer role is just reduced to searching and connecting modules. Only IC designers delve into the complexity of hardware design. Do you agree with me or can you explain why I’m wrong, please?

My question arises because I’m considering whether or not to move to hardware design from firmware. Currently, I’ve a master's in Electronic Engineering but I’m working as a firmware designer for microcontrollers."

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 2 years ago

    I don't agree - while you see  a great many published designs executed in this way this is because their is little protectable (or saleable) IP embedded in them.

    Real products made commercially still (often) use original hardware design to gain cost and performance advantage. But having invested a lot of money in a design it's not usually a good plan to publish it.

    The picture shows an example (a current project):

    There are two processors and an FPGA but there are filters ADCs, bipolar DACs, switching supplies, differential amplifiers etc. None of these are copies of reference designs (although obviously based on the huge body of analogue design knowledge available in books, on the internet etc.).

    And while I can happily show you a picture of the pcb I'm not ready to share the detailed design.

    image

    There will be work for good hardware designers for a long time - and I suggest that such work is much more resistant to attack by AI  than any kind of software work.

    MK

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • acdc90
    acdc90 over 2 years ago in reply to michaelkellett

    Hello, My job for the last 38years is repairing electronics. when dealing with domestic equipment which can sometimes get circuits. But when i am doing industrial modules i have never got circuits. so using data sheets and my own test points works. one thing that gets me is when designed they put small caps running 24/7 in a standby power supply that should be away from heat. Where i have found bigger caps of the same value last longer.

    then a motor driver ic with multiple legs would die because it has high voltage then dust then moisture.

    When you plan power supply or Driver circuits do you think of the life of caps in the machine  

    running 24/7 there is 8760 hours in the first year of warrantee 

    how many caps used are better than 2,000 hours.

      

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • acdc90
    acdc90 over 2 years ago in reply to michaelkellett

    Hello, My job for the last 38years is repairing electronics. when dealing with domestic equipment which can sometimes get circuits. But when i am doing industrial modules i have never got circuits. so using data sheets and my own test points works. one thing that gets me is when designed they put small caps running 24/7 in a standby power supply that should be away from heat. Where i have found bigger caps of the same value last longer.

    then a motor driver ic with multiple legs would die because it has high voltage then dust then moisture.

    When you plan power supply or Driver circuits do you think of the life of caps in the machine  

    running 24/7 there is 8760 hours in the first year of warrantee 

    how many caps used are better than 2,000 hours.

      

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 2 years ago in reply to acdc90
    acdc90 said:
    When you plan power supply or Driver circuits do you think of the life of caps in the machine  

    Actually, yes.

    The board in the picture will have an easy life - it's planned existence is that, after development and testing, it's powered up life time will be << 1000 hours.

    But that is unusual.

    You can make your caps last longer by running them cool and de-rating by large factors for voltage and ripple. 1000 hour rated cheap caps often last a very long time in low stress applications.

    The realities of power design often result in large stress on capacitors but when the cost of a big 10000 hour 450V cap can exceed £100 you can see why they don't end up in washing machines.

    Another thing to watch out for is that the capacitance of ceramic capacitors (especially Y5U and X5R types) can be as little as 20% of nominal value at the full rated voltage and less than 50% of nominal at 50% of rated voltage.

    Good point about the dust !

    Just been working on a design with 80V supply and lots of tracks -  0.15mm track and gap rules definitely not suitable !

    MK