Products
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
Member's Forum Raspberry Pi, Microsoft, and USB Flash Drives (memory devices).
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 628 subscribers
  • Views 847 views
  • Users 0 members are here
Related

Raspberry Pi, Microsoft, and USB Flash Drives (memory devices).

electronicbiker
electronicbiker over 2 years ago

Hi Guys, ElectronicBiker here, with a problem.

I have a PC, a RISC-PC, and several Raspberry Pi's. Sometimes I need to transfer files between a raspberry Pi and the PC, sometimes back again. The files are usually .TXT or .JPG. Taking a USB memory device out of a Raspberry Pi and plugging it into the PC generates a fault message with the recommendation that I allow windoze to scan and repair the device. I have to allow this to happen, so I do. Most of the time the memory device works on both the PC and the Pi, occasionally it cannot be repaired so windoze does something to it that makes it unusable on any machine.

I know that the Pi runs Linux, which started life some time in the 70's or 80's (I think), I also know that changes are made every so often. Unfortunately I also know that microsoft windoze is the global standard for unfathomable reasons. So why can't a version of the file handling software be created for Linux that works reliably on a windoze machine as well?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 2 years ago

    I cannot remember the last time I used a USB memory stick with a Pi, but don't recall an issue; my daily desktop machine is a Windows PC. However, as mentioned by others, if your machines are connected, then it's much simpler usually to use the network. Many SSH clients will have SFTP capability built-in (or use command line). I use SecureCRT a lot, but it's paid software (but excellent, well worth it).

    image

    Or, another free option,, just directly from PowerShell, you can use 'sftp'.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago

    I cannot remember the last time I used a USB memory stick with a Pi, but don't recall an issue; my daily desktop machine is a Windows PC. However, as mentioned by others, if your machines are connected, then it's much simpler usually to use the network. Many SSH clients will have SFTP capability built-in (or use command line). I use SecureCRT a lot, but it's paid software (but excellent, well worth it).

    image

    Or, another free option,, just directly from PowerShell, you can use 'sftp'.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • electronicbiker
    0 electronicbiker over 2 years ago in reply to shabaz

    Thanks shabaz, I'll give it a try!