Products
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
Member's Forum Raspberry Pi, Microsoft, and USB Flash Drives (memory devices).
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 628 subscribers
  • Views 847 views
  • Users 0 members are here
Related

Raspberry Pi, Microsoft, and USB Flash Drives (memory devices).

electronicbiker
electronicbiker over 2 years ago

Hi Guys, ElectronicBiker here, with a problem.

I have a PC, a RISC-PC, and several Raspberry Pi's. Sometimes I need to transfer files between a raspberry Pi and the PC, sometimes back again. The files are usually .TXT or .JPG. Taking a USB memory device out of a Raspberry Pi and plugging it into the PC generates a fault message with the recommendation that I allow windoze to scan and repair the device. I have to allow this to happen, so I do. Most of the time the memory device works on both the PC and the Pi, occasionally it cannot be repaired so windoze does something to it that makes it unusable on any machine.

I know that the Pi runs Linux, which started life some time in the 70's or 80's (I think), I also know that changes are made every so often. Unfortunately I also know that microsoft windoze is the global standard for unfathomable reasons. So why can't a version of the file handling software be created for Linux that works reliably on a windoze machine as well?

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 2 years ago

    an other option (as mentioned by SensoredHacker0 ) is to use an scp client on your windows PC. Instructions here.

    After logging in, you 'll get an interface like this, with your PC filesystem(s) left, and the Raspberry filesystem right.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 2 years ago in reply to Jan Cumps

    I concur with JC. Using network conductivity to move data might be easier.

    Go download the program Putty. A Windows supported suite of secure shell programs. This will give you the program pscp a secure copy program. You can use this to copy programs from windows to Linux and scp to copy from Linux to Windows over a network connection. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 2 years ago in reply to Jan Cumps

    I concur with JC. Using network conductivity to move data might be easier.

    Go download the program Putty. A Windows supported suite of secure shell programs. This will give you the program pscp a secure copy program. You can use this to copy programs from windows to Linux and scp to copy from Linux to Windows over a network connection.