Member's Forum Question of the Month: How often do you use a Handheld Oscilloscope?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 589 subscribers
  • Views 102285 views
  • Users 0 members are here
  • Handheld oscilloscope
  • oscilloscope
  • question of the month
Related

Question of the Month: How often do you use a Handheld Oscilloscope?

vivekvelusamy
vivekvelusamy over 1 year ago

e14 Question of the Month

Engineers are on the go. Gone are the days when engineers do most of their work in the lab or on the bench. They use test equipment in the facility or at a job site, that is, out of the ordinary locations. For these settings, engineers need handheld, portable equipment to make precise, accurate measurements. Handheld oscilloscopes are the focus of this month's Question of the Month: How often do you use a Handheld Oscilloscope?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 1 year ago +3
    Some pros and cons for hand-held scopes: Hand-held Pros Portable - can be used in mobile applications Isolated - useful when you don't want the instrument grounded to mains ground Small - useful…
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Instructorman +3
    How would you define reasonably capable? The one I have, is comparable to a 100 MHz 2 channel bench scope like the Rigol 1102 for generic use and usability (including screen resolution). Except for elaborate…
  • obones
    obones over 1 year ago +2
    As a hobbyist, I have somewhat limited resources so between the antique CRT based unmovable Telequipment D1011 scope and the DSO Shell 150, I find myself using the latter more often that not.
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to manojroy123
    manojroy123 said:
    Depends upon project to project

    What are the dependencies? When do you go for handheld vs bench?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vmate
    vmate over 1 year ago

    Although I've never had a nice handheld scope, ever since I got my DHO804, which can be powered from an external battery bank with USB-C, I don't feel the need to get or use a handheld one. It's small enough to carry around, although larger than handheld scopes, it's so much nicer to use than a portable one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago

    I have a couple of handheld oscilloscopes. None of them are high-end, but they are surprisingly capable, for a lot of use cases.

    I originally thought that I'd be only using them only for "field" work, and for the rare occasions where I'm not near my bench-top scopes, but turns out I've found myself using them even when I have my other scopes at arm's reach.

    Handheld oscilloscopes are normally simpler, so they boot instantly and require less fiddling with settings, so for a quick inspection they are quite efficient.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 1 year ago

    Some pros and cons for hand-held scopes:

    Hand-held Pros

    • Portable - can be used in mobile applications
    • Isolated - useful when you don't want the instrument grounded to mains ground
    • Small - useful in setups where there is little space for instrumentation
    • Video framing - can be used in images and videos of apparatus where you need to show the scope display without it dominating the image area

    Hand-held Cons

    • Not high performance - limited bandwidth, limited resolution, limited accuracy, limited voltage
    • Cramped, non-standard controls
    • Small cables, connectors and probes that may have limited performance and can be pretty flimsy
    • Small low-res screen - hard to see some signal features
    • Poor triggering
    • Few channels
    • Batteries die

    USB scope Pros

    • Save on the cost of a display (if you have a host computer already)
    • Can have a nice display with extensive processing capabilities

    USB scope Cons

    • Slow boot
    • Limited performance
    • Non-standard controls
    • More cables
    • Can take a lot of space to place the host computer

    I'm sure members can add more pros and cons in the comments below.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to dougw

    This may only apply to the lower end of the market, but...

    One feature of the USB scope I particularly like is the 'panoramic' width of the waveform display.

    You can display the whole capture and still be able to read the text on the protocol decoding overlay. Hit the 'print screen' and you have a copy of it stored for later.

    On the bench scope, by the time you are zoomed in enough to read the decoding, then you have to pan back and forth to see the rest of the captured waveform. The screen capture option tends to limit you to a copy of the current viewport and not of the the whole capture. So you have to pan, screen capture, pan, screen capture, pan, screen capture... then download and stitch the individual images back together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • taifur
    taifur over 1 year ago

    I don't have a handheld oscilloscope but I believe it is very effective for everyday use. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Instructorman
    Instructorman over 1 year ago

    I would use a handheld 'scope more often if I owned one.  I am currently evaluating the available product offerings, hoping to find a handheld that is both affordable and reasonably capable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Instructorman

    How would you define reasonably capable?

    The one I have, is comparable to a 100 MHz 2 channel bench scope like the Rigol 1102 for generic use and usability (including screen resolution). Except for elaborate triggering. That's more difficult on my handhold.

    Action photo: capture timer pulse of a GPS, while I try to configure the behaviour of said pulse:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Jan Cumps
    Jan Cumps said:
    Except for elaborate triggering. That's more difficult on my handhold.

    A return to the old external trigger box days.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • aspork42
    aspork42 over 1 year ago

    I got one here from a Project 14 prize and it is nice. Used it for probing mains connected boards and for troubleshooting while up on a ladder. Much better that way than with my bench scope. But usually the bench scope is better. I think the portable scope is more of a “second scope” for someone who already has a decent bench scope.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>