Member's Forum What're you up to this weekend?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 55 replies
  • Subscribers 628 subscribers
  • Views 4870 views
  • Users 0 members are here
  • weekend plans
Related

What're you up to this weekend?

cstanton
cstanton over 2 years ago

I'm going to tinker with different soundcards I have, USB and PCI to see which is better at storing and playing audio from old vinyl records that I have.

What do/don't you have planned?

  • Sign in to reply
  • Cancel
Parents
  • javagoza
    javagoza over 2 years ago

    Honestly, I have no ear for music. I like USB sound cards. I think they are more versatile.

    This weekend I will work in this one: Eye On Intelligence Challenge 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to javagoza
    javagoza said:
    I like USB sound cards. I think they are more versatile

    They can have quirks, some certainly cap the frequencies lower than they claim; but I have an older USB Creative Soundblaster with a pre-amp that's useful for vinyl recording Slight smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to cstanton

    RIAA?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • anniel747
    anniel747 over 2 years ago in reply to cstanton

    RIAA?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • electronicbiker
    electronicbiker over 2 years ago in reply to anniel747

    I use an old auto-changer with a BSR Monarch deck and a crystal cartridge, it's good enought for most of the ex-juke-box gramophone records I get these days. The equalisation for the cartridge is a 470K resistor in series. I've also used it for 78RPM shellac records, one of which was labelled '80 RPM' but it sounded ok to my old ears. Another of the 78's tried to take the cartridge right to the centre due to an over-enthusiastic run-out groove so I had to edit a slow fade to zero at the end.

    For 33.333 LP's I use the 'line output' on the hi-fi set-up in the living-room with the original magnetic cartridge, so I don't need to bother with external equalisation units.

    I have a Word table with the details of each track (about 6,500 now). This was started several years ago, it didn't add much more time because the records had to be played in real-time anyway so I had about 3 minutes per track to do it. This data, via a Raspberry Pi, enabled me to add the meta-data to each digitised track in seconds. I still like watching the data on the display scrolling forwards and backwards while an old  78 complete with pops, clicks, oodles of stereo surface hiss plays through, high-pitched wobbly voices sounding as if the singers each have a plum in their mouths...  Little things, etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to anniel747

    newer TTs have the RIAA built in. It's also possible to filter in Audacity.