Products
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
Member's Forum More old mains sockets removed
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 625 subscribers
  • Views 2343 views
  • Users 0 members are here
Related

More old mains sockets removed

Workshopshed
Workshopshed over 1 year ago

Just swapped out these old sockets. Never seen anything quite like the bottom one. The earth was wrapped around a plate rather than having its own screw terminal.

image

I searched up the patent.

https://patents.google.com/patent/GB449631A/en

449,631. Plug couplings. ARNOLD, C. L., and DOWSETT, R. W., and MK. ELECTRIC, Ltd., Wakefield Street, Edmonton, London. Fab. 12, 1935, No. 4495. [Class 38 (i)] A socket fitting has a protector 8 that covers the supply sockets 2 and is moved in a plane by the earthing-pin 9a after it has entered its socket 3 so as to uncover the sockets 2. The projection 6a enters the socket 3 below its entry end and a guide 6b slides in holes in the socket 3 and in a plate 4a attached thereto, a spring 7 acting to keep the protector normally in the position shown. In modifications the sliding protector is furnished with a pair of limbs guided on parallel rods and interengaging with a similar pair of fixed limbs supporting the rods, springs being inserted between the limbs, or it may be guided in a channel in the base or in a cap thereon.

  • Sign in to reply
  • Cancel
Parents
  • phoenixcomm
    phoenixcomm over 1 year ago

     Workshopshed imageonly thing I can say is thank god I dont live in the UK! 220 mains~ that will kill you if you get wrapped up in it. I have been bitten by US mains (120) and Im still here!! When I lived in Asbury Park I lived in a Victorian, and did rehab on it. First problem was Knob and Tubing, then no safety ground, ouch. This pic from my house in Farmers Branch, North Dallas. The SOB used a doubled up single box and had the wires bare going from one box to another.  Plus the ground wire, bare-bright copper ground never went to the send box. I don't think the switches had grounds. But the use of the two boxes instead of double gang and the stunt with the wires where VERBOTEN!.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 1 year ago in reply to phoenixcomm

    Been shocked a couple of times with 240v whilst working on a prototype light dimmer. Luckily the RCD triggered and although very shaken I wasn't dead. My testing approach has changed significantly since then.

    However, having seen US electrics, I would suggest you stick with 110v.

    We do have special "site" transformers which bring the voltage down to 110v or as I recently discovered it's actually plus/minus 50v.

    Although I believe the US system is actually a centre tap off 240v to give you the 110v.

    Our main breaker here is just 100A which is pretty standard here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to Workshopshed

     Workshopshed  imageSorry when I talk about 120/110 Its one half of the 240 so you end up with 240 main = {Hot-120} + Neutral +  {Hot-120} the 240 is handled by the main beaker which is on both poles! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • acdc90
    acdc90 over 1 year ago in reply to phoenixcomm

    another fright is from when we had Hotels with VCR's

    walk into a hotel with 40 rooms to work on aerial system

    aerial was earthed with roof 

    there was 1 brand of VCR that had 5m ohm resister between phase and neutral to body

    so you got to wear it when you unplugged the  aerial amplifier  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • acdc90
    acdc90 over 1 year ago in reply to phoenixcomm

    another fright is from when we had Hotels with VCR's

    walk into a hotel with 40 rooms to work on aerial system

    aerial was earthed with roof 

    there was 1 brand of VCR that had 5m ohm resister between phase and neutral to body

    so you got to wear it when you unplugged the  aerial amplifier