Member's Forum More old mains sockets removed
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 625 subscribers
  • Views 2294 views
  • Users 0 members are here
Related

More old mains sockets removed

Workshopshed
Workshopshed over 1 year ago

Just swapped out these old sockets. Never seen anything quite like the bottom one. The earth was wrapped around a plate rather than having its own screw terminal.

image

I searched up the patent.

https://patents.google.com/patent/GB449631A/en

449,631. Plug couplings. ARNOLD, C. L., and DOWSETT, R. W., and MK. ELECTRIC, Ltd., Wakefield Street, Edmonton, London. Fab. 12, 1935, No. 4495. [Class 38 (i)] A socket fitting has a protector 8 that covers the supply sockets 2 and is moved in a plane by the earthing-pin 9a after it has entered its socket 3 so as to uncover the sockets 2. The projection 6a enters the socket 3 below its entry end and a guide 6b slides in holes in the socket 3 and in a plate 4a attached thereto, a spring 7 acting to keep the protector normally in the position shown. In modifications the sliding protector is furnished with a pair of limbs guided on parallel rods and interengaging with a similar pair of fixed limbs supporting the rods, springs being inserted between the limbs, or it may be guided in a channel in the base or in a cap thereon.

  • Sign in to reply
  • Cancel
  • acdc90
    acdc90 over 1 year ago in reply to phoenixcomm

    another fright is from when we had Hotels with VCR's

    walk into a hotel with 40 rooms to work on aerial system

    aerial was earthed with roof 

    there was 1 brand of VCR that had 5m ohm resister between phase and neutral to body

    so you got to wear it when you unplugged the  aerial amplifier  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • acdc90
    acdc90 over 1 year ago in reply to phoenixcomm

    In Australia and New Zealand with 240v MEN (multiple earth neutral) where each house has its own earth and that is connected to the comon neutral at each house works fine when you grow up with it 

    then in most houses before 1970 you had 2 phases ( to share the load ) as it was 3 phase on the pole 

    so when looking at 3ph this is 415 between 2 phases 

    when it gets scarey is when the neutral becomes disconnected between the house and the pole

    EG turn on 1000w stove element (from phase A) and 150w tv and light on (from phase b)  

    so with no neutral the 230v tv gets 415v and dies. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to anniel747

     anniel747  My house in Farmers Branch (N. Dallas) did in fact have Orangeburg!  I had my sewer line cleaned out 4 or 5 time. the last time my plumber said no-more replace the line! we dug it up and it was broken in 3 or 4 spots and the so called clean up was just a stick of PVC jammed into the pipe..while the offending Orangeburg was removed I picked up the supplies I also decided to replace the gas line as well. installed it the inspector came by the next day and blessed it but need a 24hr gas pressure test.  passed that too. covered it all in. do you know where the gas leek came from? Nope Not the Clothes drier, or the Water heater, nor the gas stove or oven. I came from my front yard gas lamp! I picked up a new lamp but still had the dam leek. there was a valve in the line to the lamp. replaced the valve! No more leek. could have save the change of the lamp and really the new line itself! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to anniel747

     anniel747 said: "Same guy worked on that half?"  image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to phoenixcomm
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to phoenixcomm
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to kmikemoo

     kmikemoo Not in new construction, But it did happen to me twice. once when I lived in Princeton, NJ. the  house used Wire-mold  (metal) all around the house the problem that he assumed the metal stayed a 'good" ground!! when I use the metal conduit or Wire-mold I always with out exception a bare-bright!!! The other time I was living in LA by the beach but worked for Hughes Aircraft. I was doing both sustaining engineer of the Satellite ATE, and support in the High Bay where we worked on the birds there were normally about 8 or so in the bay at any one time  and my lab was connected the high bay they used to come to me with problems, They had a brand new hp spectrum analyzer that was rack mounted and It would not say running it would reboot and when they got it back from test equipment repair, the problem persisted. So I was asked to look at it as they really needed the beast. well I plugged it in put an antenna  on it and listened to FM!! The next day it was still running so I told them to come and get it, and it passed with flying colors. later that day they came back and told me it rebooted again. I grabbed my Fluke and went to the high bay. I opened the back of the rack it was a maze of alligator clips and wire! I basically said WTF! And while leaning on the rack with one hand and the other on the clip. Well I got knocked to the floor. I told them I would return a little later and pulled out the 100a pull-out. I went upstairs to my boss and told him what happened, I told him what I thought was wrong, he promptly agreed.  I grabbed a 100a lock-out device, and called the guy in charge of the gantry crane!  Remember I was doing sustaining? I was for the ATE's Power Controller unit which was under the floor! Meanwhile back on the floor as my jack-stands appeared (floor was about 10x10') and the crane started moving Flight came down to find out what the hell I was doing. as my boss was over flight as we controlled the high-bay I told him to call my boss. At that time we attached the rings to the ATE system and started to lift it. The RF-guy came over and ask the same thing he said I would damage the wave guide. so I told him to uncouple it. I got the box opened up and saw was the ass-holes did. In the Box there Is a 100A breaker, and a 100+A RFI filter. CAN YOU GUESS WHAT WAS WRONG! Should be Pull-Out, RFI  Filter, Circuit Beaker... NOPE they had in Pull-Out, Circuit Beaker, RFI Filter. and one side shorted to ground.. I went upstairs to my office and grabbed out of a new box the RFI-Filter, and Circuit Breaker. Replaced them both and check to system, shut it down and REMOVED THE RATS NEST of Gator Clips!! ~~ Cris BTW each one of the ATE in the bay was Inspected half where wired wrong!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to Workshopshed

     Workshopshed  imageSorry when I talk about 120/110 Its one half of the 240 so you end up with 240 main = {Hot-120} + Neutral +  {Hot-120} the 240 is handled by the main beaker which is on both poles! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to anniel747

     anniel747 NOPE NOT MINE! A-HOLE WHO BUILT IT. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 1 year ago

    I worked on a friend's very old house with single fabric-coated solid wires strung between insulators in the basement.  every time I touched a wire, some of the wire coating would crumble and fall off.  The hardest part was when the wires were imbedded in brick mortar and I had to re-insulate them with some tubing so they wouldn't touch and short.  Scary stuff... 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
>