Products
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
Member's Forum steppers (x4)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 627 subscribers
  • Views 2452 views
  • Users 0 members are here
  • pico
  • stepper
  • PIO
Related

steppers (x4)

Jan Cumps
Jan Cumps over 1 year ago

Can you have enough stepper motors? Maybe.

I did an investment. I had one driver IC and a good motor. I added 4 somewhat heavier motors, and 4 Allegro A4988 drivers.

image

(for my own documentation)

  • Motor Type: Bipolar Stepper
  • Step Angle: 1.8 deg.
  • Holding Torque: 40N.cm (56oz.in)
  • Rated Current/phase: 1.7A
  • Phase Resistance: 1.5Ohm±10%
  • Insulation Resistance: 100MΩ¸ Min, 500VDC
  • Insulation Strength: 500VAC for one minute
  • Physical Specification:
  • Frame Size: 42 x 42mm (1.7 inch x 1.7 inch)
  • Body Length: 40mm
  • Shaft Diameter: 5mm
  • Number of Wire Leads: 4
  • Wire Length: 400mm
  • Weight: 280g
  • Temperature rise: 80deg Max(rated current, 2 phase on)


Rood B+
Groen A-
Zwart A+
Blauw B- 

image

One more strange stepper is on its way from China:
image, 

Goal is to control them with a single Pico.

  • Sign in to reply
  • Cancel
Parents
  • Stevio73
    Stevio73 over 1 year ago

    I’ve always been curious about multiples of steppers. Could two be used in the same ‘action’ to multiply the torque or holding force?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Stevio73

    You can electrically wire motors parallel or in series. You would not need software to drive them independently in that case. Because a single step command would control both.

    Contrary to what you'd initially expect , total torque of two parallel driven steppers is lower than of a single motor. in series, the torque adds, but the maximum stepper speed lowers due to inductance increase.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 1 year ago in reply to Jan Cumps

    What if I'd wanted to use two stepper motors for both sides of a gantry system? Should I wire them in series/parallel or would it be more suitable to use two independently controlled steppers?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to obones

    A scanner that I took apart, had a single stepper (with reduction) for the scan wagon. And a toothed belt that interacted with cogwheels at both sides of the scanner. So the force was equal on both sides, but the rubber gave a bit of mechanical leeway.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to obones

    A scanner that I took apart, had a single stepper (with reduction) for the scan wagon. And a toothed belt that interacted with cogwheels at both sides of the scanner. So the force was equal on both sides, but the rubber gave a bit of mechanical leeway.