Member's Forum Does AI plagiarize and take credit for work of others ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 627 subscribers
  • Views 1635 views
  • Users 0 members are here
Related

Does AI plagiarize and take credit for work of others ?

robogary
robogary over 1 year ago

I was surfing the web for advice on remedies for python error "module missing" and then for example code to compare to.

Later I did the same google on my cell phone, which AI wants first shot to answer. It told me " here is code from AI" , which looks exactly like example code from an older webpage. 

I was thinking , Mr AI if you found this code in cyberspace, why didn't you give the originator get credit ? It's not like they asked you for money.

I wonder if AI does the same for recipes. ......

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 1 year ago

    Here's a function, done with an AI that revealed zero sources throughout.
    I used AI to help me write this function last night. And, obviously, I guided it throughout the process to ensure I wasn't copying anyone else, so as not to violate other people's licenses.

    It's my work. With the benefits of AI. I'd be very curious if any human being can conclude it is not original work, provided they can give at least some evidence that it may have been copied from other people's work (I'll settle for just fair plausibility, I'm not looking for extreme "beyond reasonable doubt" level of evidence). It shouldn't be too hard, there are several MAX7219 libraries on GitHub that AI might have copied from (or that humans could have directly copied from pre-AI).

    void Max7219::setRamPixel(uint16_t x, uint16_t y, uint8_t pixelvalue) {
        uint16_t idx;
        uint8_t bitIdx;
        uint16_t linx, liny;
        // x position is 0..(8*mHorizQty - 1), y position is 0..(8*mVertQty - 1)
        if (mDisplayData == nullptr) return; // Ensure display data is initialized
        if (x >= 8 * mHorizQty || y >= 8 * mVertQty) return; // Validate x and y positions
        // each byte in mDisplayData represents a row of 8 pixels
        // transformation:
        // linx and liny represent the positions if the modules were all in a sigle line
        linx = (((mVertQty-1)-(y/8))*mHorizQty*8) + x;
        liny = (y % 8);
        // now do the calculations using the transformed linx and liny, i.e.
        // as if all modules were on a single 8x8 line
        idx = (linx/8) + (liny * mQty); // Calculate RAM byte index in the display data
        bitIdx = (uint8_t)(7 - (linx % 8)); //Calculate bit index within the byte, where most significant bit is at position 0
        if (pixelvalue) {
            mDisplayData[idx] |= (1 << bitIdx); // Set the pixel
        } else {
            mDisplayData[idx] &= ~(1 << bitIdx); // Clear the pixel
        }
    }
    

    And, incidentally, I can give fair evidence that it is my work (just so that the challenge is balanced, I'm not asking for anything unreasonable!).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 1 year ago in reply to shabaz

    This mostly happens when using Gemini Code Assist in VS Code. It highlights potential issues re licensing.
    image

    In my opinion, the best way around some of this minefield, is to place an acknowledgement in the header stating that the code was AI generated etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to BigG

    I'm using JetBrains IDEs, and just noticed they have a Gemini plug-in, I'll have to give it a try too.

    Occasionally AI has been quite helpful with arrays such as the ones you show; I tend to 'force' my desired encoding for the first few values, and then it figures out the pattern from there, and continues it (not always successfully, but enough to help save time overall).

    I'm also finding I'm commenting my code a lot better than pre-AI, since that acts as a guide too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 1 year ago in reply to BigG

    I'm using JetBrains IDEs, and just noticed they have a Gemini plug-in, I'll have to give it a try too.

    Occasionally AI has been quite helpful with arrays such as the ones you show; I tend to 'force' my desired encoding for the first few values, and then it figures out the pattern from there, and continues it (not always successfully, but enough to help save time overall).

    I'm also finding I'm commenting my code a lot better than pre-AI, since that acts as a guide too.