Products
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
Member's Forum MP710086 change input voltage from 110V to 240V
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 627 subscribers
  • Views 1369 views
  • Users 0 members are here
Related

MP710086 change input voltage from 110V to 240V

rsjawale24
rsjawale24 over 1 year ago

As the title suggests, I need to change the input AC voltage of Multicomp Pro MP710086 bench top power supply from 110V to 240V AC.

I received this power supply as one of the prizes in the Hackster holidays giveaway but they sent me a model with 110V AC operating supply. 

I tried taking a look at the back panel and there doesn't seem to be a voltage change switch. Is there any switch inside the supply? Or any other way to change the input voltage?

I cannot use it as the supply in my country is 240V AC.

Pictures for reference below. 

imageimage

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 1 year ago

    Looks like the only task is to change the fuse:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 1 year ago

    Looks like the only task is to change the fuse:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rsjawale24
    0 rsjawale24 over 1 year ago in reply to Jan Cumps

    No, the transformer is specifically designed for 110V AC input. The power supply has a toroidal transformer with no specs written on it. 

    For example- I opened up the soldering station and this is what is written on the transformer.
    All these units also come with US plugs. I have modular socket at my home so plugs are not an issue but the operating voltage is. 

    The transformer takes 110V AC, steps down to 24V AC for the soldering iron and 9V AC for the PCB Panel with LCD. There is a small bridge rectifier near the 9V connector. 

    I'm thinking, if I can simply replace this transformer with a 240V AC to 24V AC at least the soldering iron will work and I will bypass the AC connector and connect 9VDC supply to the panel. 

    image                image