Member's Forum Question of the Month: What’s the most frustrating part of working with modern micro-controllers?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 626 subscribers
  • Views 3439 views
  • Users 0 members are here
  • poll
  • QOM
  • question of the month
Related

Question of the Month: What’s the most frustrating part of working with modern micro-controllers?

cstanton
cstanton over 1 year ago

Micro-controllers are at the core of most embedded systems, but working with them isn’t always smooth. From confusing datasheets to fragmented tool-chains, even experienced engineers can hit roadblocks. This month, we want to know:

Bonus question:

What micro-controllers are you currently using? (and why that one?)

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 1 year ago

    Reading all of this makes me think of a few things

    I've been programming and coding since 1976, starting with PDP8 and 11, 8080 in the form of an S100 bus system configured for industrial control and even a little cobol on the company mainframe. since then probably coded in dozens of languages over the years, mainly changing because the new job had X as the standard, I think if you know how to design a good program it becomes easier to code it for a specific MCU/CPU

    Even after over 50 years I still drop to C++ as my goto with C# when targeting MS platforms.

    I like the abstraction from hardware to user code of things like the arduino IDE, its hard to say the board is an arduino anymore but I really like the code abstraction, 99% or more of applications dont need the speed of assembly or other direct platform written code and were you need a bit more power you can switch out the hardware with little change to you actual code, were you do then drop to C++ or something.

    on the STM development environment I love the configurator/mapper that allows internal function blocks to be configured and or mapped to external pins in some cases almost any pin, that's awesome and can aid in pcb layout tremendously i think.

    Distributed computing / environment is the way to go for all but the simpler systems, even now with 3D printing or other CNC/motion control type solutions there are apps like Klipper that abstract the G Code interpretation and hans of just motion control to one or more MCU's for the various parts of in my canse the 3D printer.

    I am building 2 right now, a Voron Trident and a Voron V2 R2.4, both have a PI or equivalent for the master controller and then in my case a RPI2040 based head controller for hotend temp, filament flow, cooling fans and the like, then another RPI2040 running the A/B motors for the core XY motion platform, then an ST32xxx based board running the heated bed, 3 or 4 Z motors , system cooling and various other things. The PI is also providing web interface and local display / controls.

    That's all for just a 3D printer but it keeps everything simple, the environment is abstracted but highly optimized for near real time control of those motors (Gotta make sure those circles are actually round :) ) and it supports loads of different MCU's and hardware interfaces.

    I could go on but I digress, I will be creating posts for the 3D printer builds in detail soon but thats were im at for now with coding and building.

    Oh... yes im old too Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 1 year ago

    Reading all of this makes me think of a few things

    I've been programming and coding since 1976, starting with PDP8 and 11, 8080 in the form of an S100 bus system configured for industrial control and even a little cobol on the company mainframe. since then probably coded in dozens of languages over the years, mainly changing because the new job had X as the standard, I think if you know how to design a good program it becomes easier to code it for a specific MCU/CPU

    Even after over 50 years I still drop to C++ as my goto with C# when targeting MS platforms.

    I like the abstraction from hardware to user code of things like the arduino IDE, its hard to say the board is an arduino anymore but I really like the code abstraction, 99% or more of applications dont need the speed of assembly or other direct platform written code and were you need a bit more power you can switch out the hardware with little change to you actual code, were you do then drop to C++ or something.

    on the STM development environment I love the configurator/mapper that allows internal function blocks to be configured and or mapped to external pins in some cases almost any pin, that's awesome and can aid in pcb layout tremendously i think.

    Distributed computing / environment is the way to go for all but the simpler systems, even now with 3D printing or other CNC/motion control type solutions there are apps like Klipper that abstract the G Code interpretation and hans of just motion control to one or more MCU's for the various parts of in my canse the 3D printer.

    I am building 2 right now, a Voron Trident and a Voron V2 R2.4, both have a PI or equivalent for the master controller and then in my case a RPI2040 based head controller for hotend temp, filament flow, cooling fans and the like, then another RPI2040 running the A/B motors for the core XY motion platform, then an ST32xxx based board running the heated bed, 3 or 4 Z motors , system cooling and various other things. The PI is also providing web interface and local display / controls.

    That's all for just a 3D printer but it keeps everything simple, the environment is abstracted but highly optimized for near real time control of those motors (Gotta make sure those circles are actually round :) ) and it supports loads of different MCU's and hardware interfaces.

    I could go on but I digress, I will be creating posts for the 3D printer builds in detail soon but thats were im at for now with coding and building.

    Oh... yes im old too Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • DAB
    DAB over 1 year ago in reply to Robert Peter Oakes

    No Peter, you are still a youngster.

    I am old, I started with vacuum tubes.