Member's Forum As a designer, how do you make choices?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 627 subscribers
  • Views 2831 views
  • Users 0 members are here
  • LED driver
  • designer choices
Related

As a designer, how do you make choices?

dougw
dougw over 1 year ago

A very common practice when designing with MCUs is to dedicate at least one MCU pin to drive a diagnostic or indicator LED.

There are several simple circuits that can accomplish this function. I am curious to know if  most designers use the same circuit, and if not, why not? 

Edit by cstanton : I liked this post so much I decided to elevate it to Question of the Month for August (Close enough for UK time zone anyway!)


Leave a comment that explains how it came about that you use a particular circuit.

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 1 year ago

    I have been using  NeoPixel Mini 3535 RGB LEDs as my go to indicator on my boards.  At < $0.20 in quantity of 100, it is cheap enough, and the RGB capability gives me a bit more flexibility. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 1 year ago in reply to genebren

    Cool method. How many lines of code does it take to make it indicate something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 1 year ago in reply to dougw

    Coding in 'C' it takes about 18 lines of code to send the serial string to the NeoPixel, which I do with a bit-banged IO port (pin).  There is an additional overhead to build the string, which is 3 lines of code for each color intensity change.  The programming string is 24 bits, for the 3 LED intensities, GRB ordering, 8 bits each. The timing is pretty critical, so the code must run with interrupts off (or at least make sure that the code can run without being interrupted).  A 'zero' is .2 to .4 us high time, while a 'one' is .58 to 1.0 us.

    Doing this with bit-banged IO, there are some changes to the code that need to be made to account for the microprocessor clock speed.  As the clock speed increases, you need to add additional 'NOP' commands to keep the clocking rates correct.

    Sure, it is easier to just toggle a pin, but using smaller microprocessors, pin are at a premium.  Being able to 'blink' in different colors is a nice added feature.  Also, the NeoPixels are daisy chainable, so multiple LEDs can be driven off the same pin.

    I have a client that wanted 256 level programmable RGB LEDs for his project and theses are cheaper that other approaches.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 1 year ago in reply to dougw

    That is so true.  I have used this same code (with timing modification) is several products/projects.  I really try to re-use code wherever possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 1 year ago in reply to dougw

    That is so true.  I have used this same code (with timing modification) is several products/projects.  I really try to re-use code wherever possible.