Member's Forum Is General Artificial Intelligence a Breakthrough or just a Financial Hype?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 626 subscribers
  • Views 1650 views
  • Users 0 members are here
  • ai
Related

Is General Artificial Intelligence a Breakthrough or just a Financial Hype?

HKPhysicist
HKPhysicist 8 months ago

According to my understanding, AI hype big corps spend a whole country's energy resource to produce learning software and hardware which can do a very little things for us.  Laughing

On the other hands, a parrot can learn how to talk with men with just a few grams of nutrition.  Also, my little puppy learnt how to do simple house hood things for me in just a few minutes and a few grams fo nutrition. Blush

Which one of these examples are more intelligent and energy efficient?

Had we better use those astronomical sum of money and resources on investigating deeper natural laws such as room temperature superconductivity, novel material and crystal, higher energy experiments beyond the Large Hadron Collider, nuclear fusion experiments, etc.?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz 8 months ago

    People (including some tech experts) thought the cloud was hype and a fad, and it took less than a decade for it to become crazy to not use the cloud for most businesses. Others assumed IoT was useless, and yet there are now hundreds of devices all around you wherever you go, being monitored or controlled over combined wireless and Internet, from energy meters to vending machines. Probably around 60% of my search engine queries have now been replaced by LLM interaction, it just works better. I use AI to help me with all manner of tasks (non-technical and technical).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller 8 months ago in reply to shabaz

    Personally, I still think cloud is crazy without homomorphic encryption. Businesses are risking their IP, at least, by putting control over it in the hands of others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 8 months ago in reply to bradfordmiller

    I don't know enough to comment with much authority, but I think that most orgs consider the encryption enough of a solved problem. The orgs get to control where their data resides, and almost all orgs have to trust other orgs to transport their data anyway (I.e. even if they were not using cloud, but just moving data to a redundant site they themselves own - and most of it even used to be unencrypted links if it wasn't on the public Internet), until Snowdon era.

    From what little I've seen, orgs with a tremendous amount to lose, such as banks, trust the cloud (not all PaaS features, but a large enough subset) for implementing services, and they trust the public Internet for their customers to perform online banking and commerce. (Of course, as mentioned we know since Snowdon that all that data flows through certain rooms, so nothing is 100% certain).

    The cloud providers cannot decrypt (or claim they cannot) the data belonging to businesses who are using their secure technologies. Governments also use the cloud (admittedly only specific data centers owned by the cloud providers).

    I'm not sure how homomorphicness helps, I'd need more input because I'm no subject-matter expert at all. I had a job interview one time for a firm that wished to do something like that (they didn't call it that at least to me) for medical data (since it's highly desirable to look for health trends and anomalies if only it could be done without providing health records that are traceable to individuals, except once it is known for sure that some of those individuals need to be contacted in a matter of life or death, and then it needs to be reversible by the original data owners), but I think they will have difficulty marketing it, because to me it seemed high risk that something would eventually leak, let alone the issues of getting governments to allow such transfer of data to orgs for data mining, and talking to their mathematicians, didn't give me a warm feeling (granted they were talking to a non-expert, plus I was not an employee). 

    I wish I knew more than this vagueness of my current knowledge, I'd like to learn more through self study, but I suspect I'd end up stuck as soon as I hit any reasonably difficult maths.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 7 months ago in reply to bradfordmiller


    Mobile, so I can't write much. Theoretically anything can be vulnerable (especially when there are ultimately humans involved somewhere in a transaction or workflow or process. But as mentioned, the fact is banks trust cloud with trillions and they do process data within the cloud, not merely store data. For practical purposes, the threat today is not so severe to prevent such massive volumes of commerce, with any decent solution. Same with governments using the cloud. Security will have to evolve as threats evolve. The biggest threat, well beyond limitations of today's security capabilities with any reasonably architected solution, may well be self-extinction of their own enterprise if businesses do not consider using the cloud. But this feels like a 2000's conversation, businesses have migrated (well, apart from particular industries/verticals that are traditionally slow-moving or have complex legacy systems; they may have only partially migrated), it's been a couple of decades. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller 7 months ago in reply to shabaz

    I agree that "most orgs consider encryption enough of a solved problem", but that doesn't mean it is. If you are only storing in the cloud, and you encrypt before uploading using post-quantum cryptography, you are right, that should be safe enough for some time. However, once you are using the cloud to actually perform operations on your data, it decrypts it, leaving it vulnerable both to the insider threat of employees of the cloud provider, but also side channel attacks, etc. that potentially let others get access to your data while decrypted. (Not to mention that the keys had to be in the cloud as well). Homomorphic encryption allows processing the data *while it is encrypted*, thus even the server has no idea what functions it is performing, what the input or output really are, etc. Only you, the data owner, get the result and then decrypt it on your end (not in the cloud). Or have a "private cloud" which really means your org owns and controls the servers too so can implement additional security mechanisms (like only allowing your own software to run on them, have control over vetting employees who can access the servers, etc.)

    Unfortunately, to date, while there have been some proof of concept experiments (keeping in mind the efficiency of known homomorphic algorithms is abysmal), it's still considered an impractical approach which is why I don't think cloud is practical for any non-public data processing until appropriate algorithms are discovered. Meanwhile, one can process on the edge, upload sanitized summaries if needed for sharing, and otherwise leverage cloud only for highly encrypted backups. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bradfordmiller
    bradfordmiller 7 months ago in reply to shabaz

    I agree that "most orgs consider encryption enough of a solved problem", but that doesn't mean it is. If you are only storing in the cloud, and you encrypt before uploading using post-quantum cryptography, you are right, that should be safe enough for some time. However, once you are using the cloud to actually perform operations on your data, it decrypts it, leaving it vulnerable both to the insider threat of employees of the cloud provider, but also side channel attacks, etc. that potentially let others get access to your data while decrypted. (Not to mention that the keys had to be in the cloud as well). Homomorphic encryption allows processing the data *while it is encrypted*, thus even the server has no idea what functions it is performing, what the input or output really are, etc. Only you, the data owner, get the result and then decrypt it on your end (not in the cloud). Or have a "private cloud" which really means your org owns and controls the servers too so can implement additional security mechanisms (like only allowing your own software to run on them, have control over vetting employees who can access the servers, etc.)

    Unfortunately, to date, while there have been some proof of concept experiments (keeping in mind the efficiency of known homomorphic algorithms is abysmal), it's still considered an impractical approach which is why I don't think cloud is practical for any non-public data processing until appropriate algorithms are discovered. Meanwhile, one can process on the edge, upload sanitized summaries if needed for sharing, and otherwise leverage cloud only for highly encrypted backups. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz 7 months ago in reply to bradfordmiller


    Mobile, so I can't write much. Theoretically anything can be vulnerable (especially when there are ultimately humans involved somewhere in a transaction or workflow or process. But as mentioned, the fact is banks trust cloud with trillions and they do process data within the cloud, not merely store data. For practical purposes, the threat today is not so severe to prevent such massive volumes of commerce, with any decent solution. Same with governments using the cloud. Security will have to evolve as threats evolve. The biggest threat, well beyond limitations of today's security capabilities with any reasonably architected solution, may well be self-extinction of their own enterprise if businesses do not consider using the cloud. But this feels like a 2000's conversation, businesses have migrated (well, apart from particular industries/verticals that are traditionally slow-moving or have complex legacy systems; they may have only partially migrated), it's been a couple of decades.