Member's Forum What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 71 replies
  • Subscribers 593 subscribers
  • Views 11750 views
  • Users 0 members are here
  • element14 community
  • win
  • element14 members
  • aske14
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition

E14Alice
E14Alice 1 month ago

A new month means a new AskE14!

Engineers, makers, and problem‑solvers are always finding smarter ways to work. From optimising workflows to automating repetitive tasks, small habits can add up to serious time savings.

This month, AskE14 is all about sharing the habits that help you work more efficiently, whether you’re designing, prototyping, debugging, documenting, or managing projects.

Time for the question:

What’s the most time-saving habit you’ve picked up? 

Time is a valuable resource in engineering. A simple habit — like better version control, smarter test setups, or clearer documentation. This can save hours down the line.

imageimage

Competition Details

You'll have to be a member of the element14 Community to join in and take part in this “Join, Share & Win” challenge. It's simple, all you have to do is:


1. You need to make sure you are  Register  or Login
2. Then answer the following question by adding a reply or commenting!

What’s the most time-saving habit you’ve picked up? 

This month, we are giving away:

The Community team will then select the best 3 answers to win the UNO R4 Minima! 

image

Closing date: 1st March 

Winners announced: 10th March 

UNO R4 Minima  

Terms and Conditions 

imagePDF

The winners! 

dang74 

wolfgangfriedrich 

skruglewicz 

E14Alice will be reaching out to you soon to confirm contact details

  • Cancel

Top Replies

  • dang74
    dang74 1 month ago +5
    For hobby projects I've been pasting code into ChatGPT so that it can fulfill the role of a peer review. It has caught many dumb mistakes that would have otherwise gone unnoticed until the debug stage…
  • Arnovsharma
    Arnovsharma 1 month ago +5
    The habit that has been most valuable to me is to document my work as I do it, rather than later. This includes: Maintaining a simple project log (even in a notebook or text file). Recording why…
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago +5
    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation…
  • dang74
    dang74 1 month ago

    For hobby projects I've been pasting code into ChatGPT so that it can fulfill the role of a peer review.  It has caught many dumb mistakes that would have otherwise gone unnoticed until the debug stage.

    • Cancel
    • Vote Up +5 Vote Down
    • Cancel
  • Arnovsharma
    Arnovsharma 1 month ago

    The habit that has been most valuable to me is to document my work as I do it, rather than later.

    This includes:

    • Maintaining a simple project log (even in a notebook or text file).
    • Recording why I made a particular design decision.
    • Recording pin connections, jumper settings, and test results.
    • Saving versions of schematics, code, and PCB files with descriptive names.

    Why this saves time:
    When I return to a project after several weeks or months, I don’t have to try to figure out what I did. I can simply pick up where I left off.

    • Cancel
    • Vote Up +5 Vote Down
    • Cancel
  • Aniket_kumar_raj
    Aniket_kumar_raj 1 month ago

    The most time saving thing ever done in my life was organising all stuffs cuz as a tech guy there is a mess really on cupboard and table,which makes it harder to find things, like if I say you to find a male to male jumper wire then you won't be able to without a deep adventure in the abyss

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago

    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation fails, the hardware will fail for sure. 

    • Cancel
    • Vote Up +5 Vote Down
    • Cancel
  • Aniket_kumar_raj
    Aniket_kumar_raj 1 month ago in reply to dang74

    That's too relatable, I think almost everyone here does this

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Aniket_kumar_raj
    Aniket_kumar_raj 1 month ago in reply to Arnovsharma

    I am sure it's AI generated

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • Aniket_kumar_raj
    Aniket_kumar_raj 1 month ago in reply to wolfgangfriedrich

    Woh, that's what I need to, what's the simulation software is called,I used tinkercad but that for limited

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • rsc
    rsc 1 month ago

    The most time-saving habit I've picked up is to add the date/revision to a filename when I save it.  ...and remembering to put the connector shell on the cable before soldering it.....

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • battlecoder
    battlecoder 1 month ago

    My biggest time-saving habit is organizing projects better; breaking them into smaller steps on a board; separated by "pending", "in progress" and "completed".

    Now, maybe this is different for other people, but this saves me a lot of time because normally trying to "reconnect" and resume a project is a very slow process for me (reviewing where I was with the schematic, or the code, or the prototyping, etc). This is specially true when I'm working on more than one project at a time (which is sometimes unavoidable) or when I can't work on a project for an entire week. Having a quick, immediate way of knowing where I was and what comes next helps me resume my work almost immediately.

    This also helps me figure out ahead of time what things can be done immediately, and what steps can't be tackled right now or have requirements that need to be met first (like ordering parts), further assisting me in making better use of my time.

    Generally speaking, planning and "thinking ahead"; writing down lists of steps, decisions, requirements, etc (and crossing off those that are completed, done, etc) has become an invaluable habit in working efficiently, both at home as well as at work.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • battlecoder
    battlecoder 1 month ago in reply to rsc

    If its not the connector shell it's the heatshrink, isn't i? At this point I should put that on a sticker and place it right in front of me on my bench.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
>